<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 Quad MIPI CSI 2 Multiple Device Interfacing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-MIPI-CSI-2-Multiple-Device-Interfacing/m-p/542479#M85487</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anuradha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if this will work, at least seems it was not tested.&lt;/P&gt;&lt;P&gt;However feasible option would be multiplex these&amp;nbsp; streams in an FPGA. &lt;/P&gt;&lt;P&gt;Each stream in this case should use a different stream identifier (stream 0-3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 23:57:42 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-19T23:57:42Z</dc:date>
    <item>
      <title>IMX6 Quad MIPI CSI 2 Multiple Device Interfacing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-MIPI-CSI-2-Multiple-Device-Interfacing/m-p/542478#M85486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a video processing application we are intending to use an HDMI and a CVBS analog camera inputs with IMX6 Quad processor. ADV7481 is an ideal solution to achieve both requirements through MIPI CSI 2 bus, however in ADV7481 HDMI and CVBS inputs are connected to two separated MIPI transmitters (4 lane for HDMI and a single lane for CVBS) and driven by two separated differential clock signals. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, can we interface these two separated transmitter signals to single MIPI CSI 2 input of the IMX6 processor ? Let's say we configure the HDMI output to be 1 lane MIPI (out of 4), so we have clkp/clkn, d0p/d0n for HDMI and&amp;nbsp; by default clkp/clkn, d0p/d0n for CVBS output. Can these two differential clk lines be tied together ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 09:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-MIPI-CSI-2-Multiple-Device-Interfacing/m-p/542478#M85486</guid>
      <dc:creator>tengri</dc:creator>
      <dc:date>2016-08-19T09:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Quad MIPI CSI 2 Multiple Device Interfacing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-MIPI-CSI-2-Multiple-Device-Interfacing/m-p/542479#M85487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anuradha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if this will work, at least seems it was not tested.&lt;/P&gt;&lt;P&gt;However feasible option would be multiplex these&amp;nbsp; streams in an FPGA. &lt;/P&gt;&lt;P&gt;Each stream in this case should use a different stream identifier (stream 0-3).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 23:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Quad-MIPI-CSI-2-Multiple-Device-Interfacing/m-p/542479#M85487</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-19T23:57:42Z</dc:date>
    </item>
  </channel>
</rss>