<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FlexCAN single shot mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542289#M85466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Single shot mode (also know as one-shot mode) is a transmission mode which will try to send a can frame only once ( no automatic retransmission if there is a transmission error ). For more information about single shot mode you can se SJA1000 manual (&lt;A href="http://www.nxp.com/documents/application_note/AN97076.pdf" title="http://www.nxp.com/documents/application_note/AN97076.pdf"&gt;http://www.nxp.com/documents/application_note/AN97076.pdf&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are developing can protocol stacks and in order to implement a time triggered protocol on imx6, we would like to know if single shot feature is available on the can controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Madjid&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 08:49:37 GMT</pubDate>
    <dc:creator>madjidlho</dc:creator>
    <dc:date>2016-08-19T08:49:37Z</dc:date>
    <item>
      <title>FlexCAN single shot mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542289#M85466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Single shot mode (also know as one-shot mode) is a transmission mode which will try to send a can frame only once ( no automatic retransmission if there is a transmission error ). For more information about single shot mode you can se SJA1000 manual (&lt;A href="http://www.nxp.com/documents/application_note/AN97076.pdf" title="http://www.nxp.com/documents/application_note/AN97076.pdf"&gt;http://www.nxp.com/documents/application_note/AN97076.pdf&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are developing can protocol stacks and in order to implement a time triggered protocol on imx6, we would like to know if single shot feature is available on the can controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Madjid&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 08:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542289#M85466</guid>
      <dc:creator>madjidlho</dc:creator>
      <dc:date>2016-08-19T08:49:37Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN single shot mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542290#M85467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, there is no Single Shot Transmission feature implemented in the FlexCAN module of the i.MX6 series processors. Only regular Transmission Abort operation can be performed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 09:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542290#M85467</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-08-22T09:13:27Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN single shot mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542291#M85468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur, thanks for your fast answer.&lt;/P&gt;&lt;P&gt;Do you know if it is possible to detect arbitration lost with flexCan?&lt;/P&gt;&lt;P&gt;thanks for your feedback.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 12:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542291#M85468</guid>
      <dc:creator>madjidlho</dc:creator>
      <dc:date>2016-08-22T12:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN single shot mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542292#M85469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The FlexCAN module can detect and signal the transmission error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 11:30:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FlexCAN-single-shot-mode/m-p/542292#M85469</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-08-24T11:30:21Z</dc:date>
    </item>
  </channel>
</rss>