<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6SL Android 4.4.2 EVK USB Camera preview callback not enabled issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SL-Android-4-4-2-EVK-USB-Camera-preview-callback-not/m-p/542265#M85465</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Suguna,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you check what kind of Camera it is using the ZBarScanner-master application and zxing-android-embedded-master applications,&amp;nbsp; I think if you are getting the error in the Camera HAL it is because the CAMERA need to be configure in a way to get the application the info,&amp;nbsp; is the camera crashing also with the photo android based application?&amp;nbsp; Did you register the USB Camera in the configuration file? what was the process you follow to add the camera can you share?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Oct 2016 15:46:05 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2016-10-07T15:46:05Z</dc:date>
    <item>
      <title>i.MX6SL Android 4.4.2 EVK USB Camera preview callback not enabled issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SL-Android-4-4-2-EVK-USB-Camera-preview-callback-not/m-p/542264#M85464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our requirement is to read different barcodes (1D, 2D like QRcode, PDF417 ...etc) using 5mp USB camera.&lt;/P&gt;&lt;P&gt;Processor : 1.MX6SL&lt;/P&gt;&lt;P&gt;Target Board : EVK&lt;/P&gt;&lt;P&gt;OS : Android 4.4.2 BSP&lt;/P&gt;&lt;P&gt;Camera: USB 5mp truly make&lt;/P&gt;&lt;P&gt;Connected : USB OTG port of EVK board&lt;/P&gt;&lt;P&gt;Camera config: &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; setprop back_camera_name uvc&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; setprop back_camera_orient 0&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We tested with ZBarScanner-master application and zxing-android-embedded-master applications.&lt;/P&gt;&lt;P&gt;Both are failing in Camera HAL layer (disableMsgType 0x10, Preview callback not enabled 10, enableMsgType 0x10, Disabling Preview Callback).&lt;/P&gt;&lt;P&gt;Please find attached log with zbar cam for your reference.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly suggest us to resolve the issue.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Malleswari&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336592"&gt;Camera.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 06:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SL-Android-4-4-2-EVK-USB-Camera-preview-callback-not/m-p/542264#M85464</guid>
      <dc:creator>malleswari</dc:creator>
      <dc:date>2016-08-19T06:52:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SL Android 4.4.2 EVK USB Camera preview callback not enabled issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SL-Android-4-4-2-EVK-USB-Camera-preview-callback-not/m-p/542265#M85465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Suguna,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you check what kind of Camera it is using the ZBarScanner-master application and zxing-android-embedded-master applications,&amp;nbsp; I think if you are getting the error in the Camera HAL it is because the CAMERA need to be configure in a way to get the application the info,&amp;nbsp; is the camera crashing also with the photo android based application?&amp;nbsp; Did you register the USB Camera in the configuration file? what was the process you follow to add the camera can you share?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Oct 2016 15:46:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SL-Android-4-4-2-EVK-USB-Camera-preview-callback-not/m-p/542265#M85465</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2016-10-07T15:46:05Z</dc:date>
    </item>
  </channel>
</rss>