<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: cfimager error -22 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542013#M85434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karl-Johan &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you try :&lt;/P&gt;&lt;P&gt;cfimager.exe -f ./output/mx28/bin/mx28-obds.sb -d g&amp;nbsp; &lt;/P&gt;&lt;P&gt;(use -a option for the first time when format is needed)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 20 Aug 2016 00:00:34 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-20T00:00:34Z</dc:date>
    <item>
      <title>cfimager error -22</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542012#M85433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having problems with a custom board with an i.MX28 processor (see &lt;A _jive_internal="true" href="https://community.nxp.com/message/653838?et=watches.email.thread#comment-653838"&gt;https://community.nxp.com/message/653838?et=watches.email.thread#comment-653838&lt;/A&gt;). I have a theory that the problem is related to the flash memory, so I want to run the i.MX28 On-Board Diagnostics Suite. I have built the obds binary and am trying to flash it to an SD-card with cfimager (part of the obds package). The command I've run and its output is as follows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt;cfimager.exe -f mx28-obds.sb -d h -a&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Failed to unlock drive, closing anyway!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error: error -22&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've failed to find any information of what error -22 means. Can someone here help me figure it out?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an alternative to cfimager?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 10:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542012#M85433</guid>
      <dc:creator>thekarl</dc:creator>
      <dc:date>2016-08-19T10:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager error -22</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542013#M85434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Karl-Johan &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you try :&lt;/P&gt;&lt;P&gt;cfimager.exe -f ./output/mx28/bin/mx28-obds.sb -d g&amp;nbsp; &lt;/P&gt;&lt;P&gt;(use -a option for the first time when format is needed)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Aug 2016 00:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542013#M85434</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-20T00:00:34Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager error -22</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542014#M85435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That command gives me the same output, so I don't think it's the -a option that is the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SD-card i'm trying to flash is formatted as FAT32, if that matters.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Aug 2016 06:44:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542014#M85435</guid>
      <dc:creator>thekarl</dc:creator>
      <dc:date>2016-08-22T06:44:56Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager error -22</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542015#M85436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the cause for the failure to unlock the drive. The program did not run with admin rights. When it's run as admin, wrting to the sd card works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I've run in to aother problem. When I try to boot the device from the sd card I get the following output on the usb debug interface:&lt;/P&gt;&lt;P&gt;HTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;BR /&gt;Undefined InsHTLLCLLJ&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The Undefined InsHTLLCLLJ part repeats forever.&lt;/P&gt;&lt;P&gt;Is something wrong with the boot image?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 09:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542015#M85436</guid>
      <dc:creator>thekarl</dc:creator>
      <dc:date>2016-08-24T09:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: cfimager error -22</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542016#M85437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; The "Undefined Ins" message may be caused because of memory bug.&lt;/P&gt;&lt;P&gt;Also please take a look at the next thread :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/334321"&gt;What does 'Undefined Ins' mean in u-boot?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 04:24:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/cfimager-error-22/m-p/542016#M85437</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-10-13T04:24:55Z</dc:date>
    </item>
  </channel>
</rss>