<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 LAN7500 and imx6, how to implement</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541814#M85402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have imx6 Board. &lt;/P&gt;&lt;P&gt;on the Board i have LAN7500 chip. LAN7500 connected to imx6 USB2. Over menuconfig I included driver for LAN7500. After boot I connected Ethernet cable to LAN7500 and can see, that Ethernet Link is OK(LEDs lihtning). But if I try ping some address in Internet - Linux say me "bad address". I suppose, that I have to make some more steps to implement LAN7500. &lt;/P&gt;&lt;P&gt;Which steps have to be done(LAN 7500 driver is already included in .config) for full funktionality LAN7500 with imx6.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jun 2016 05:59:43 GMT</pubDate>
    <dc:creator>alexlevandovski</dc:creator>
    <dc:date>2016-06-17T05:59:43Z</dc:date>
    <item>
      <title>LAN7500 and imx6, how to implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541814#M85402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have imx6 Board. &lt;/P&gt;&lt;P&gt;on the Board i have LAN7500 chip. LAN7500 connected to imx6 USB2. Over menuconfig I included driver for LAN7500. After boot I connected Ethernet cable to LAN7500 and can see, that Ethernet Link is OK(LEDs lihtning). But if I try ping some address in Internet - Linux say me "bad address". I suppose, that I have to make some more steps to implement LAN7500. &lt;/P&gt;&lt;P&gt;Which steps have to be done(LAN 7500 driver is already included in .config) for full funktionality LAN7500 with imx6.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 05:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541814#M85402</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-17T05:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LAN7500 and imx6, how to implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541815#M85403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had you set correct mac address ?&lt;/P&gt;&lt;P&gt;&lt;A href="https://en.wikibooks.org/wiki/Changing_Your_MAC_Address/Linux" title="https://en.wikibooks.org/wiki/Changing_Your_MAC_Address/Linux"&gt;Changing Your MAC Address/Linux - Wikibooks, open books for an open world&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 06:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541815#M85403</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-17T06:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: LAN7500 and imx6, how to implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541816#M85404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&amp;nbsp; and thanks for Answer. No, I did'nt nothing - only included a driver to Linux image. How can I set mac address in boot procedure, that my Board after boot get ready to go in Internet without extra configuration from user?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 06:32:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541816#M85404</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-17T06:32:52Z</dc:date>
    </item>
    <item>
      <title>Re: LAN7500 and imx6, how to implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541817#M85405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to p.7,9 LAN7500 datasheet&lt;/P&gt;&lt;P&gt;&lt;A href="http://ww1.microchip.com/downloads/en/DeviceDoc/7500.pdf" title="http://ww1.microchip.com/downloads/en/DeviceDoc/7500.pdf"&gt;http://ww1.microchip.com/downloads/en/DeviceDoc/7500.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 07:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541817#M85405</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-17T07:29:57Z</dc:date>
    </item>
    <item>
      <title>Re: LAN7500 and imx6, how to implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541818#M85406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this Datasheet advice, but as I wrote both LEDs are on(Link 1GB).Somewhat another are don't made. But what?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jun 2016 09:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LAN7500-and-imx6-how-to-implement/m-p/541818#M85406</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-06-17T09:39:53Z</dc:date>
    </item>
  </channel>
</rss>