<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPCIE phy link never came up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541702#M85389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I need active PCIE on my imx6 Board. On the Kernel boot I get this Information:&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers enabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then this:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# lspci&lt;/P&gt;&lt;P&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# dmesg|grep pci&lt;/P&gt;&lt;P&gt;device class 'pci_bus': registering&lt;/P&gt;&lt;P&gt;bus: 'pci': registered&lt;/P&gt;&lt;P&gt;device: '1ffc000.pcie': device_add&lt;/P&gt;&lt;P&gt;bus: 'platform': add device 1ffc000.pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': add driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': driver_probe_device: matched device 1ffc000.pcie with driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': really_probe: probing driver imx6q-pcie with device 1ffc000.pcie&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: no default pinctrl state&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;device: 'pci0000:00': device_add&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: scanning bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: supports D1&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# disabled&lt;/P&gt;&lt;P&gt;bus: 'pci': add device 0000:00:00.0&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: fixups for bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: scanning bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: fixups for bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: fixup irq: got 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: assigning IRQ 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 4 [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 5 [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;driver: '1ffc000.pcie': driver_bound: bound to device 'imx6q-pcie'&lt;/P&gt;&lt;P&gt;bus: 'platform': really_probe: bound device 1ffc000.pcie to driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver imx_pcie_ep&lt;/P&gt;&lt;P&gt;ehci-pci: EHCI PCI platform driver&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver ehci-pci&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver ci_hdrc_pci&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver TW6869&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see PCIE is not OK. is anybody know, how to get PCIE&amp;nbsp; link up?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jul 2016 12:29:41 GMT</pubDate>
    <dc:creator>alexlevandovski</dc:creator>
    <dc:date>2016-07-06T12:29:41Z</dc:date>
    <item>
      <title>PCIE phy link never came up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541702#M85389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I need active PCIE on my imx6 Board. On the Kernel boot I get this Information:&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;PCI: bus0: Fast back to back transfers disabled&lt;/P&gt;&lt;P&gt;PCI: bus1: Fast back to back transfers enabled&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then this:&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# lspci&lt;/P&gt;&lt;P&gt;00:00.0 PCI bridge: Device 16c3:abcd (rev 01)&lt;/P&gt;&lt;P&gt;root@imx6qsabresd:~# dmesg|grep pci&lt;/P&gt;&lt;P&gt;device class 'pci_bus': registering&lt;/P&gt;&lt;P&gt;bus: 'pci': registered&lt;/P&gt;&lt;P&gt;device: '1ffc000.pcie': device_add&lt;/P&gt;&lt;P&gt;bus: 'platform': add device 1ffc000.pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': add driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': driver_probe_device: matched device 1ffc000.pcie with driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'platform': really_probe: probing driver imx6q-pcie with device 1ffc000.pcie&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: no default pinctrl state&lt;/P&gt;&lt;P&gt;imx6q-pcie 1ffc000.pcie: phy link never came up&lt;/P&gt;&lt;P&gt;device: 'pci0000:00': device_add&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: scanning bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: supports D1&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PME# disabled&lt;/P&gt;&lt;P&gt;bus: 'pci': add device 0000:00:00.0&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: fixups for bus&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: scanning bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: fixups for bus&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: bus scan returning with max=01&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: fixup irq: got 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: assigning IRQ 155&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: BAR 6: assigned [mem 0x01100000-0x0110ffff pref]&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to [bus 01]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 4 [io&amp;nbsp; 0x1000-0x10000]&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: resource 5 [mem 0x01000000-0x01efffff]&lt;/P&gt;&lt;P&gt;driver: '1ffc000.pcie': driver_bound: bound to device 'imx6q-pcie'&lt;/P&gt;&lt;P&gt;bus: 'platform': really_probe: bound device 1ffc000.pcie to driver imx6q-pcie&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver imx_pcie_ep&lt;/P&gt;&lt;P&gt;ehci-pci: EHCI PCI platform driver&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver ehci-pci&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver ci_hdrc_pci&lt;/P&gt;&lt;P&gt;bus: 'pci': add driver TW6869&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see PCIE is not OK. is anybody know, how to get PCIE&amp;nbsp; link up?&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 12:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541702#M85389</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-07-06T12:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE phy link never came up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541703#M85390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;had you tried other pcie modules, are they linked.&lt;/P&gt;&lt;P&gt;It may be useful to check sugestions on&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="376261" data-objecttype="1" href="https://community.nxp.com/thread/376261"&gt;https://community.nxp.com/thread/376261&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and patches on &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fmessage%2F518226%23518226" rel="nofollow" target="_blank"&gt;https://community.freescale.com/message/518226#518226&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 00:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541703#M85390</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-07T00:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE phy link never came up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541704#M85391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor, in the first Link I'm already wrote my question. I Can't find what to do with "phy link never came up"".&lt;/P&gt;&lt;P&gt;Second Link probably help me if I get link "PCIE: imx_pcie_pltfm_probe start link up.", but I don't know..&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 08:04:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PCIE-phy-link-never-came-up/m-p/541704#M85391</guid>
      <dc:creator>alexlevandovski</dc:creator>
      <dc:date>2016-07-07T08:04:03Z</dc:date>
    </item>
  </channel>
</rss>