<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eCompass on iMX6 SDB board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eCompass-on-iMX6-SDB-board/m-p/541621#M85384</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. The Sabre SDB board comes with the same MAG3110 Magnetometer and MMA8451Q Accelerometer?&lt;/P&gt;&lt;P&gt;A. Yes, the i.MX6SX SABRE SD board comes with the MAG3110 magnetometer and MMA8451Q accelerometer.&lt;/P&gt;&lt;P&gt;Q. Has anyone found a source or guide on how to port the eCompass libraries from the Kinetics platform to the M4 core on a iMX6SX.&lt;/P&gt;&lt;P&gt;A. There is no such a procedure. You have to write your own software, using the existing I2C drivers of the Linux BSP to access the sensors.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 11:44:16 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-08-25T11:44:16Z</dc:date>
    <item>
      <title>eCompass on iMX6 SDB board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eCompass-on-iMX6-SDB-board/m-p/541620#M85383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone found a source or guide on how to port the eCompass libraries from the Kinetics platform to the M4 core on a iMX6SX. The Sabre SDB board comes with the same MAG3110 Magnetometer and MMA8451Q Accelerometer?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 08:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eCompass-on-iMX6-SDB-board/m-p/541620#M85383</guid>
      <dc:creator>jameshall</dc:creator>
      <dc:date>2016-08-19T08:09:38Z</dc:date>
    </item>
    <item>
      <title>Re: eCompass on iMX6 SDB board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eCompass-on-iMX6-SDB-board/m-p/541621#M85384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. The Sabre SDB board comes with the same MAG3110 Magnetometer and MMA8451Q Accelerometer?&lt;/P&gt;&lt;P&gt;A. Yes, the i.MX6SX SABRE SD board comes with the MAG3110 magnetometer and MMA8451Q accelerometer.&lt;/P&gt;&lt;P&gt;Q. Has anyone found a source or guide on how to port the eCompass libraries from the Kinetics platform to the M4 core on a iMX6SX.&lt;/P&gt;&lt;P&gt;A. There is no such a procedure. You have to write your own software, using the existing I2C drivers of the Linux BSP to access the sensors.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 11:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eCompass-on-iMX6-SDB-board/m-p/541621#M85384</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-08-25T11:44:16Z</dc:date>
    </item>
  </channel>
</rss>