<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UART Receiving Problem IMX6Q bare-metal programming   in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541164#M85347</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Khaled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at attached example for i.MX6Q Sabre board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Aug 2016 23:51:17 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-08-19T23:51:17Z</dc:date>
    <item>
      <title>UART Receiving Problem IMX6Q bare-metal programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541163#M85346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All, &lt;BR /&gt;I tried to configure the UART peripheral in IMX6Q using the reference manual Chapter64 section 13.1&lt;/P&gt;&lt;P&gt;with header "Programming the UART in RS-232 mode" i just made little changes with control flow to make it a software instead of hardware and the baud rate also the RXFIFO trigger level to 1 character instead of 30&lt;BR /&gt;In the main program:&lt;BR /&gt;i tried to write directly to the UTXD register &lt;BR /&gt;and the output correctly appeared.&lt;BR /&gt;and i tried in an infinite loop to read any data from URXD register and then forward it to the UTXD&lt;/P&gt;&lt;P&gt;but when trying to write anything to the console there is no thing happened and i receive nothing.&lt;BR /&gt;_________________________________________________________________________________________________________&lt;BR /&gt;so can anyone help me figure out what is the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i even tried to see the registers using the jtag connection with Dstream device but all memory locations are accessible except for the &lt;BR /&gt;UART registerts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 13:19:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541163#M85346</guid>
      <dc:creator>khaledali</dc:creator>
      <dc:date>2016-08-19T13:19:06Z</dc:date>
    </item>
    <item>
      <title>Re: UART Receiving Problem IMX6Q bare-metal programming</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541164#M85347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Khaled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at attached example for i.MX6Q Sabre board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Aug 2016 23:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541164#M85347</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-19T23:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: UART Receiving Problem IMX6Q bare-metal programming </title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541165#M85348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks igor i'll try to see the differences between the 2 configurations &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Aug 2016 08:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UART-Receiving-Problem-IMX6Q-bare-metal-programming/m-p/541165#M85348</guid>
      <dc:creator>khaledali</dc:creator>
      <dc:date>2016-08-20T08:06:56Z</dc:date>
    </item>
  </channel>
</rss>