<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX 6 Sabrelite</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-Sabrelite/m-p/538602#M85209</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently facing some problems with mxc_v4l2_tvin.out test in IMX6Q sabrelite. My system configuration is as follows:&lt;/P&gt;&lt;P&gt;1. LTIB version : L3.0.35_4.1&lt;/P&gt;&lt;P&gt;2. Ubuntu 14.04&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem:&lt;/P&gt;&lt;P&gt;I am interfacing adv7180 decoder to the sabrelite card through IPU0-&amp;gt;CSI0, the drivers are loaded properly, then when i run mxc_v4l2_tvin test the output the output is also displayed on the screen; but after some time the output gets blank. So pls provide some suggestions to overcome the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vignesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Jul 2016 12:55:12 GMT</pubDate>
    <dc:creator>vigneshp</dc:creator>
    <dc:date>2016-07-05T12:55:12Z</dc:date>
    <item>
      <title>IMX 6 Sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-Sabrelite/m-p/538602#M85209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently facing some problems with mxc_v4l2_tvin.out test in IMX6Q sabrelite. My system configuration is as follows:&lt;/P&gt;&lt;P&gt;1. LTIB version : L3.0.35_4.1&lt;/P&gt;&lt;P&gt;2. Ubuntu 14.04&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem:&lt;/P&gt;&lt;P&gt;I am interfacing adv7180 decoder to the sabrelite card through IPU0-&amp;gt;CSI0, the drivers are loaded properly, then when i run mxc_v4l2_tvin test the output the output is also displayed on the screen; but after some time the output gets blank. So pls provide some suggestions to overcome the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Vignesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 12:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-Sabrelite/m-p/538602#M85209</guid>
      <dc:creator>vigneshp</dc:creator>
      <dc:date>2016-07-05T12:55:12Z</dc:date>
    </item>
    <item>
      <title>Re: IMX 6 Sabrelite</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-6-Sabrelite/m-p/538603#M85210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vignesh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try to disable blanking&lt;/P&gt;&lt;P&gt;&lt;A href="https://freescale.jiveon.com/thread/329043" title="https://freescale.jiveon.com/thread/329043"&gt;Disable screen blanking on i.MX6 running Yocto | NXP Community&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2016 00:13:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-6-Sabrelite/m-p/538603#M85210</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-06T00:13:19Z</dc:date>
    </item>
  </channel>
</rss>