<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Interfacing SSP1_DATA3 in imx287</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-SSP1-DATA3-in-imx287/m-p/538470#M85202</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, the SSP1_DATA3 pin is not used for any boot purpose on the i.MX28 EVK board. However, lease note that it is used as the Power Enable GPIO signal for the Ethernet PHYs on the EVK board. So, be aware of possible conflict between Ethernet and ADC operation if using this pin for the ADC interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jun 2016 12:17:43 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2016-06-24T12:17:43Z</dc:date>
    <item>
      <title>Interfacing SSP1_DATA3 in imx287</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-SSP1-DATA3-in-imx287/m-p/538469#M85201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using imx287 EVK board with Linux 2.6.35 and also developing prototype board. On this board we are connecting ADC and there will be no need for audio and LCD pins.&lt;/P&gt;&lt;P&gt;ADC is 24-bit and connection are as follow:&lt;/P&gt;&lt;P&gt;ADC select line (DRDY)- SSP1_DATA3&lt;/P&gt;&lt;P&gt;ADC o/p line (DOUT) - SSP3_MIS0&lt;/P&gt;&lt;P&gt;ADC SCLK - SSP3_ SCK&lt;/P&gt;&lt;P&gt;ADC CS - SSP3_SS0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In one of the blog &lt;A _jive_internal="true" href="https://community.nxp.com/message/346045#comment-346045" title="https://community.nxp.com/message/346045#comment-346045"&gt;https://community.nxp.com/message/346045&lt;/A&gt;&amp;nbsp; I seen that SSP1_DATA3 is used as Boot for imx23. Is it same case for imx287?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bhavesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 08:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-SSP1-DATA3-in-imx287/m-p/538469#M85201</guid>
      <dc:creator>bkpatel</dc:creator>
      <dc:date>2016-06-16T08:05:11Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing SSP1_DATA3 in imx287</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-SSP1-DATA3-in-imx287/m-p/538470#M85202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, the SSP1_DATA3 pin is not used for any boot purpose on the i.MX28 EVK board. However, lease note that it is used as the Power Enable GPIO signal for the Ethernet PHYs on the EVK board. So, be aware of possible conflict between Ethernet and ADC operation if using this pin for the ADC interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jun 2016 12:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-SSP1-DATA3-in-imx287/m-p/538470#M85202</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-06-24T12:17:43Z</dc:date>
    </item>
  </channel>
</rss>