<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックFrozen source mode in SDMA ( imx51)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Frozen-source-mode-in-SDMA-imx51/m-p/538199#M85179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to realize the following scenario: &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;A FPGA module connected via EMI has a few FIFOs ( 16 bit ) in output ( schema in attachment ). Each of them has its own address and queue with length = x. When the queue reaches size = y ( y &amp;lt; x ), an interrupt is raised and the data are copied into circular buffers in IMX memory. I want to realize it using SDMA module. &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;In this moment I can copy the data in incremental mode but I need to &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;freeze&lt;/SPAN&gt;&lt;/SPAN&gt; source (FIFO) address and increment only destination. &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance, &lt;BR /&gt;Peter &lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Jul 2016 11:50:45 GMT</pubDate>
    <dc:creator>peterkozakiewic</dc:creator>
    <dc:date>2016-07-25T11:50:45Z</dc:date>
    <item>
      <title>Frozen source mode in SDMA ( imx51)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frozen-source-mode-in-SDMA-imx51/m-p/538199#M85179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to realize the following scenario: &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;A FPGA module connected via EMI has a few FIFOs ( 16 bit ) in output ( schema in attachment ). Each of them has its own address and queue with length = x. When the queue reaches size = y ( y &amp;lt; x ), an interrupt is raised and the data are copied into circular buffers in IMX memory. I want to realize it using SDMA module. &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;In this moment I can copy the data in incremental mode but I need to &lt;SPAN class="short_text" lang="en"&gt;&lt;SPAN&gt;freeze&lt;/SPAN&gt;&lt;/SPAN&gt; source (FIFO) address and increment only destination. &lt;BR /&gt; &lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Thank you in advance, &lt;BR /&gt;Peter &lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 11:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frozen-source-mode-in-SDMA-imx51/m-p/538199#M85179</guid>
      <dc:creator>peterkozakiewic</dc:creator>
      <dc:date>2016-07-25T11:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: Frozen source mode in SDMA ( imx51)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Frozen-source-mode-in-SDMA-imx51/m-p/538200#M85180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately i.MX51 sdma scripts have not such script&lt;/P&gt;&lt;P&gt;(sdma ap_2_ap fixed address), so it is necessary to create own script.&lt;/P&gt;&lt;P&gt;Suggest to create service request for providing ideas how it could&lt;/P&gt;&lt;P&gt;be done. Note nxp does not provide tools for writing/developing custom&lt;/P&gt;&lt;P&gt;sdma scripts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 23:46:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Frozen-source-mode-in-SDMA-imx51/m-p/538200#M85180</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-25T23:46:24Z</dc:date>
    </item>
  </channel>
</rss>