<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Does the ubuntu Image include zImage? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537189#M85117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the image includes the zImage and the device tree for the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, as I said yesterday in one of your question, you should *not* use MFGTools with our images/platforms:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/431089"&gt;iMX6 sabre lite always in download mode&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, we provide an option to flash the images under Windows if you don't have Linux:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.alexpage.de/usb-image-tool/" title="http://www.alexpage.de/usb-image-tool/"&gt;alex's coding playground » USB Image Tool&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jul 2016 08:27:45 GMT</pubDate>
    <dc:creator>gary_bisson</dc:creator>
    <dc:date>2016-07-26T08:27:45Z</dc:date>
    <item>
      <title>Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537184#M85112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I noticed that the ubuntu Image(.img.gz) available for iMX6 sabre lite board. But I don't know whether it include zImage. I downloaded the mfgtools and checked the ucl2.xml, I found the u-boot , zImage, initramfs and rootfs can be flashed into the board. My question is that is it enough to flash ubuntu Image after flashing u-boot. Should I flash the zImage separately?&lt;/P&gt;&lt;P&gt;The ubuntu Image I mentioned above is &lt;A href="https://boundarydevices.com/mx-linux-kernel-3-14-52/" title="Ubuntu Trusty for i.MX6 boards – February 2016 (kernel 3.14.28)"&gt;Ubuntu Trusty for i.MX6/7 boards – March 2016 (kernel 3.14.52) &lt;/A&gt;&lt;/P&gt;&lt;P&gt;which is located at &lt;A href="http://boundarydevices.com.commondatastorage.googleapis.com/20160330-nitrogen-3.14.52_1.1.0_ga-trusty-en_US-lxde_armhf.img" title="http://boundarydevices.com.commondatastorage.googleapis.com/20160330-nitrogen-3.14.52_1.1.0_ga-trusty-en_US-lxde_armhf.img"&gt;http://boundarydevices.com.commondatastorage.googleapis.com/20160330-nitrogen-3.14.52_1.1.0_ga-trusty-en_US-lxde_armhf.i…&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 10:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537184#M85112</guid>
      <dc:creator>xiaochao0131</dc:creator>
      <dc:date>2016-07-25T10:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537185#M85113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/gary_bisson"&gt;gary_bisson&lt;/A&gt;​ are you able to help here?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 20:30:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537185#M85113</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-07-25T20:30:07Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537186#M85114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mfgtools is just small linux image and all linux commands can be executed&lt;/P&gt;&lt;P&gt;by it (add them to ucl2.xml). So "dd" command also can be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 23:51:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537186#M85114</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-25T23:51:20Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537187#M85115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="206296" data-username="igorpadykov" href="https://community.nxp.com/people/igorpadykov"&gt;igorpadykov,&lt;/A&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;Thanks for your reply.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;I flashed uboot just now, and there is only uboot in my board, In this case, can I flash ubuntu image to my board ? &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class="number1 alt2 line index0"&gt;&lt;CODE class="shell plain"&gt;~&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;/Downloads&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;$ &lt;/CODE&gt;&lt;CODE class="functions shell"&gt;sudo&lt;/CODE&gt; &lt;CODE class="functions shell"&gt;umount&lt;/CODE&gt; &lt;CODE class="shell plain"&gt;/dev/sdc&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;*&lt;/CODE&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="number2 alt1 line index1"&gt;&lt;CODE class="shell plain"&gt;~&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;/Downloads&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;$ zcat 20160213-nitrogen*.img.gz | &lt;/CODE&gt;&lt;CODE class="functions shell"&gt;sudo&lt;/CODE&gt; &lt;CODE class="functions shell"&gt;dd&lt;/CODE&gt; &lt;CODE class="shell plain"&gt;of=&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;/dev/sdc&lt;/CODE&gt; &lt;CODE class="shell plain"&gt;bs=1M&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number3 index2 alt2 line"&gt;&lt;CODE class="shell plain"&gt;~&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;/Downloads&lt;/CODE&gt;&lt;CODE class="shell plain"&gt;$ &lt;/CODE&gt;&lt;CODE class="functions shell"&gt;sync&lt;/CODE&gt;&lt;/P&gt;&lt;P class="number3 index2 alt2 line"&gt;&lt;/P&gt;&lt;P class="number3 index2 alt2 line"&gt;&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;I have naver flashed the zImage, I don't know if the ubuntu image contains the zImage.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 02:21:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537187#M85115</guid>
      <dc:creator>xiaochao0131</dc:creator>
      <dc:date>2016-07-26T02:21:05Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537188#M85116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes these linux commands also may work, please try to add&lt;/P&gt;&lt;P&gt;them to ucl2.xml. Also please read documentation in mfg tools&lt;/P&gt;&lt;P&gt;../Document&amp;nbsp; folder.&lt;/P&gt;&lt;P&gt;For big images one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/430984"&gt;Increasing the size of initfsram for mfgtool&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 05:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537188#M85116</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-26T05:50:02Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537189#M85117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the image includes the zImage and the device tree for the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, as I said yesterday in one of your question, you should *not* use MFGTools with our images/platforms:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/431089"&gt;iMX6 sabre lite always in download mode&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, we provide an option to flash the images under Windows if you don't have Linux:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.alexpage.de/usb-image-tool/" title="http://www.alexpage.de/usb-image-tool/"&gt;alex's coding playground » USB Image Tool&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jul 2016 08:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537189#M85117</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2016-07-26T08:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537190#M85118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 01:29:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537190#M85118</guid>
      <dc:creator>xiaochao0131</dc:creator>
      <dc:date>2016-07-27T01:29:12Z</dc:date>
    </item>
    <item>
      <title>Re: Does the ubuntu Image include zImage?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537191#M85119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As Gary said above, you can use the USB Mass Storage (ums) command to flash the image, which contains the kernel and userspace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To add just a little detail:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;the board boots through the boot script (/6x_bootscript), and you can view that file with an editor if you just skip over the first bytes of binary header.&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;&lt;LI&gt;The kernel (gzipped) is accessed through the symlink /vmlinuz, which will point at a file in /boot. There are some notes about "Ubuntunizing" the kernel here: &lt;BR /&gt;&lt;A href="https://boundarydevices.com/ubuntunizing-i-mx6-kernels/" title="https://boundarydevices.com/ubuntunizing-i-mx6-kernels/"&gt;https://boundarydevices.com/ubuntunizing-i-mx6-kernels/&lt;/A&gt; &lt;BR /&gt;&lt;BR /&gt;In short: since the Boundary Devices' Ubuntu images boot through a RAM disk, you also need to update the kernel modules inside the ram disk (pointed at by /initrd.img).&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 17:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-the-ubuntu-Image-include-zImage/m-p/537191#M85119</guid>
      <dc:creator>ericnelsonaz</dc:creator>
      <dc:date>2016-07-28T17:07:35Z</dc:date>
    </item>
  </channel>
</rss>