<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6 - Parallel Camera driver for FPGA</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536789#M85047</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good evening,&lt;/P&gt;&lt;P&gt;I am working on connecting a FPGA module which deliver a YUV video signal to the IMX6q. I need to connect it using the parallel port. I am using the IPU0 + CSI0 and I have modified the IOMUX register to activate the parallel way. I am using a kernel based on the 3.14.53 release.&lt;/P&gt;&lt;P&gt;I have read the v4l2 driver, some ov5640 driver but none of them provide me some information regarding the connection of a component which does not answer to I2C. My FPGA is only sending me data in a particular format, I do not intend to change any configuration, it cannot answer to any request.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I understand the basic of the video configuration but for the detection part, I am stuck. I don't understand how to make the connection from /dev/video0 to the FPGA without I2C. Does a hard coded configuration will work ?&lt;/P&gt;&lt;P&gt;Is there anybody that can give me some help on this part ?&amp;nbsp; &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sylvain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Jul 2016 19:15:21 GMT</pubDate>
    <dc:creator>sylvainlehenaff</dc:creator>
    <dc:date>2016-07-04T19:15:21Z</dc:date>
    <item>
      <title>IMX6 - Parallel Camera driver for FPGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536789#M85047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good evening,&lt;/P&gt;&lt;P&gt;I am working on connecting a FPGA module which deliver a YUV video signal to the IMX6q. I need to connect it using the parallel port. I am using the IPU0 + CSI0 and I have modified the IOMUX register to activate the parallel way. I am using a kernel based on the 3.14.53 release.&lt;/P&gt;&lt;P&gt;I have read the v4l2 driver, some ov5640 driver but none of them provide me some information regarding the connection of a component which does not answer to I2C. My FPGA is only sending me data in a particular format, I do not intend to change any configuration, it cannot answer to any request.&amp;nbsp; &lt;/P&gt;&lt;P&gt;I understand the basic of the video configuration but for the detection part, I am stuck. I don't understand how to make the connection from /dev/video0 to the FPGA without I2C. Does a hard coded configuration will work ?&lt;/P&gt;&lt;P&gt;Is there anybody that can give me some help on this part ?&amp;nbsp; &lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sylvain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 19:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536789#M85047</guid>
      <dc:creator>sylvainlehenaff</dc:creator>
      <dc:date>2016-07-04T19:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 - Parallel Camera driver for FPGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536790#M85048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sylvain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes hard coded configuration will work, one can remove i2c references from&lt;/P&gt;&lt;P&gt;driver codes using attached Linux Manual sect.6.3 Source Code Structure,&lt;/P&gt;&lt;P&gt;Chapter 20 MIPI CSI2 Driver. Supported formats described in &lt;/P&gt;&lt;P&gt;Table 66. Camera Input Signal Cross Reference, Format, and Bits Per Cycle&lt;/P&gt;&lt;P&gt;i.MX6DQ Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some useful links:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fmessage%2F309833%23309833" rel="nofollow" target="_blank"&gt;https://community.freescale.com/message/309833#309833&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/331888" title="https://community.freescale.com/message/331888"&gt;MX53 CSI/IDMAC config for Aptina 12-bit graysca... | NXP Community&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 00:38:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536790#M85048</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-05T00:38:35Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 - Parallel Camera driver for FPGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536791#M85049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for the help, I get further but remains stop when launching the video stream. &lt;/P&gt;&lt;P&gt;I get a timeout while waiting for an interrupt&amp;nbsp; in mxc_v4l_dqueue. I have to check the configuration.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sylvain&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jul 2016 19:06:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/536791#M85049</guid>
      <dc:creator>sylvainlehenaff</dc:creator>
      <dc:date>2016-07-11T19:06:29Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 - Parallel Camera driver for FPGA</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/1205403#M167114</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Sylvain&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; sorry to bother you. But i also need help for this development.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; I have the same situation with you. Do you sovle this problem later?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; If you sovled in the end, can you give any help about this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; Thank you very much !&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;zhou&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Dec 2020 05:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Parallel-Camera-driver-for-FPGA/m-p/1205403#M167114</guid>
      <dc:creator>zhouqi</dc:creator>
      <dc:date>2020-12-31T05:47:07Z</dc:date>
    </item>
  </channel>
</rss>