<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I found ipu warning in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535145#M84961</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when I run ipu test, input is 1920x1080 raw YUYV 16bit stream, output is 1280x720 RGB888.&lt;/P&gt;&lt;P&gt;(i.mx6solo, linux 3.10.45)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see lots of:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and the screen is flickering. Reboot the machine, then run the same app, everything is ok. What's the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 03 Jul 2016 12:17:03 GMT</pubDate>
    <dc:creator>garyyin</dc:creator>
    <dc:date>2016-07-03T12:17:03Z</dc:date>
    <item>
      <title>I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535145#M84961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when I run ipu test, input is 1920x1080 raw YUYV 16bit stream, output is 1280x720 RGB888.&lt;/P&gt;&lt;P&gt;(i.mx6solo, linux 3.10.45)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see lots of:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and the screen is flickering. Reboot the machine, then run the same app, everything is ok. What's the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Jul 2016 12:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535145#M84961</guid>
      <dc:creator>garyyin</dc:creator>
      <dc:date>2016-07-03T12:17:03Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535146#M84962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try the 'dmfc=3' kernel boot-up command option. This would increase &lt;/P&gt;&lt;P&gt;display FIFO size for display per IPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2016 00:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535146#M84962</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-04T00:24:28Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535147#M84963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same problem as Gary, but the&amp;nbsp;dmfc=3 parameter didn't change anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use kernel 3.14.52 on SabreSD-like board, with&amp;nbsp;1280x720 RGB888 video output as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 22:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535147#M84963</guid>
      <dc:creator>thomasgrimault</dc:creator>
      <dc:date>2016-10-03T22:18:23Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535148#M84964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had this same problem running OpenELEC (Kodi) at 1080p and adding 'dmfc=3' fixed the problem. Sometimes the bootargs can be overridden by the uEnv.txt, so check that it is really set correctly with:&lt;/P&gt;&lt;P&gt;cat&amp;nbsp; /proc/cmdline&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Clay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Jan 2017 02:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535148#M84964</guid>
      <dc:creator>claymontgomery</dc:creator>
      <dc:date>2017-01-15T02:19:30Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535149#M84965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please provide a link to a document that explains the use of the dmfc parameter? Would using a value larger than 3 possibly increase the reliability of video play and what is the memory cost of this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Clay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Jan 2017 18:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535149#M84965</guid>
      <dc:creator>claymontgomery</dc:creator>
      <dc:date>2017-01-21T18:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535150#M84966</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; How were you playing video when you got these IPU warnings?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were you using ffmpeg, gstreamer, or what? It seems to be a problem with the IPU's scaler and some apps avoid using the IPU's scaler by using V4L2 instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Clay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jan 2017 23:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535150#M84966</guid>
      <dc:creator>claymontgomery</dc:creator>
      <dc:date>2017-01-22T23:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535151#M84967</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Clay&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to attached Release Notes Table 11. Common kernel boot&lt;/P&gt;&lt;P&gt;parameters p.23&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jan 2017 23:27:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/535151#M84967</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2017-01-22T23:27:43Z</dc:date>
    </item>
    <item>
      <title>Re: I found ipu warning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/1840112#M222100</link>
      <description>In this release note nxp mentioned that hdmi cannot be configured from kernel under known issue.</description>
      <pubDate>Wed, 03 Apr 2024 09:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-found-ipu-warning/m-p/1840112#M222100</guid>
      <dc:creator>prateek22</dc:creator>
      <dc:date>2024-04-03T09:28:18Z</dc:date>
    </item>
  </channel>
</rss>