<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I.Mx35 USB OTG Issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184746#M8479</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pranav,&lt;/P&gt;&lt;P&gt;You have to Configure the Linux Kernel to have the OTG Support.&lt;/P&gt;&lt;P&gt;You mentioned that nothing happens- What is not happening ?&lt;/P&gt;&lt;P&gt;Is it that -it is not working as a host or it is not working as a device?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Som Appu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Feb 2012 02:46:47 GMT</pubDate>
    <dc:creator>SomAppu</dc:creator>
    <dc:date>2012-02-10T02:46:47Z</dc:date>
    <item>
      <title>I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184744#M8477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I am using Freescale I.Mx35 PDK as the hardware and Linux kernel 2.6.31 as the OS.&lt;/P&gt;&lt;P&gt;I am facing some&amp;nbsp; problem with the USB OTG.&lt;/P&gt;&lt;P&gt;USB OTG should work as both Host and also as a Device, depending upon the status of The UID pin, this is not happening.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is&amp;nbsp; working:-&lt;BR /&gt;&lt;BR /&gt;1) When configured as Host, the OTG is working as a host and is also supplying the 5V power (for devices connected to it).&lt;BR /&gt;&lt;BR /&gt;2) When Configured as Device, the OTG is working as a device and does not provide the 5V power.&lt;BR /&gt;&lt;BR /&gt;3) UID Pin Status detection is working.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;What is Not Working:- &lt;BR /&gt;&lt;BR /&gt;1) When Configured as OTG Dual Role, it is not working as both Host and as a Device depending upon the status of the UID pin.&lt;BR /&gt;&lt;BR /&gt;a. OTG is working as a USB Device, when the UID Pin is pulled high.&lt;BR /&gt;&lt;BR /&gt;b. OTG is not working as a Host when the UID Pin is shorted to Ground.&lt;BR /&gt;&lt;BR /&gt;2) When the UID Pin is pulled high, it detects it and mentions that it resumes its working as Device.&lt;BR /&gt;&lt;BR /&gt;When the UID Pin is shorted to ground, it detects it and mentions that it is suspending its working as a Device, but it is not working as a Host and also not providing the power supply of 5V.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Nov 2011 08:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184744#M8477</guid>
      <dc:creator>SomAppu</dc:creator>
      <dc:date>2011-11-08T08:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184745#M8478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Som,&lt;/P&gt;&lt;P&gt;I am having issues just to use USBOTG on imx35. I build linux kernel with USBOTG; but when I connect imx35 to my PC nothing happens.&lt;/P&gt;&lt;P&gt;Is there any hardware config required to enable USBOTG ?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pranav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2012 01:43:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184745#M8478</guid>
      <dc:creator>PranavSanghadia</dc:creator>
      <dc:date>2012-02-10T01:43:55Z</dc:date>
    </item>
    <item>
      <title>Re: I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184746#M8479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pranav,&lt;/P&gt;&lt;P&gt;You have to Configure the Linux Kernel to have the OTG Support.&lt;/P&gt;&lt;P&gt;You mentioned that nothing happens- What is not happening ?&lt;/P&gt;&lt;P&gt;Is it that -it is not working as a host or it is not working as a device?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Som Appu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2012 02:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184746#M8479</guid>
      <dc:creator>SomAppu</dc:creator>
      <dc:date>2012-02-10T02:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184747#M8480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Som,&lt;/P&gt;&lt;P&gt;I have connected imx35's USBOTG port to a Linux machine's USB port.But Linux machine does not detect, I also tried connecting it to Win 7 machine, but it also did not detect new hardware.&lt;/P&gt;&lt;P&gt;I followed the process given in Chapter 19 of Reference Manual to configure USBOTG. One of the option "IRAM for USB" generates compile time erros, so I did not select it. Am I referring to the right document?&lt;/P&gt;&lt;P&gt;Can you briefly described how did you compile your kernel and any other process to make USBOTG work? If possible can you share your .config?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pranav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2012 03:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184747#M8480</guid>
      <dc:creator>PranavSanghadia</dc:creator>
      <dc:date>2012-02-10T03:48:21Z</dc:date>
    </item>
    <item>
      <title>Re: I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184748#M8481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pranav,&lt;/P&gt;&lt;P&gt;I think you are trying to configure the OTG as a device - isn't it ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; if yes - did you make any USB Gadget selection selection ?&lt;/P&gt;&lt;P&gt;i am attaching the configuration what i used , go through it - it will work as a Device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2012 06:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184748#M8481</guid>
      <dc:creator>SomAppu</dc:creator>
      <dc:date>2012-02-10T06:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: I.Mx35 USB OTG Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184749#M8482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Som,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot. It worked :-). I was able to configure OTG as device. After applying a patch I also connect a modem to IMX35 :-).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pranav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2012 22:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-Mx35-USB-OTG-Issue/m-p/184749#M8482</guid>
      <dc:creator>PranavSanghadia</dc:creator>
      <dc:date>2012-02-10T22:19:18Z</dc:date>
    </item>
  </channel>
</rss>