<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Increasing the size of initfsram for mfgtool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532560#M84773</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my question is different, when the mfgtool image boots and creates the ram image, the space available in the rootfs is only 120MiB, 20MiBare used by the files and thus only a 100MiB image can be stored in /tmp to flash the nand. I need the rootfs in RAM to be at least 200MiB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Jul 2016 01:21:53 GMT</pubDate>
    <dc:creator>valentinafernan</dc:creator>
    <dc:date>2016-07-23T01:21:53Z</dc:date>
    <item>
      <title>Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532558#M84771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to flash a 200+MB image to NAND, but the rootfs created on RAM by the MFGTOOL is only 120M, how can I increase this size?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 22:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532558#M84771</guid>
      <dc:creator>valentinafernan</dc:creator>
      <dc:date>2016-07-22T22:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532559#M84772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Valentina&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mfg tool is small linux image which is located&lt;/P&gt;&lt;P&gt;in ..Profiles/Linux/OS Firmware/firmware.&lt;/P&gt;&lt;P&gt;Images which are programmed on board are located&lt;/P&gt;&lt;P&gt;in ..Profiles/Linux/OS Firmware/files, seems there should be&lt;/P&gt;&lt;P&gt;no problem with its size. These images are build independently&lt;/P&gt;&lt;P&gt;from mfg tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 01:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532559#M84772</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-23T01:05:09Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532560#M84773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my question is different, when the mfgtool image boots and creates the ram image, the space available in the rootfs is only 120MiB, 20MiBare used by the files and thus only a 100MiB image can be stored in /tmp to flash the nand. I need the rootfs in RAM to be at least 200MiB&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 01:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532560#M84773</guid>
      <dc:creator>valentinafernan</dc:creator>
      <dc:date>2016-07-23T01:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532561#M84774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;my rootfs.ubi is around 200MiB, when my mfgtool script (ucl.xml) sends the file via USB, the file won't fit the temporary file system created by the mfgtool firmware, I need this file system to be 200MiB &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 01:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532561#M84774</guid>
      <dc:creator>valentinafernan</dc:creator>
      <dc:date>2016-07-23T01:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532562#M84775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;could you look at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-105215"&gt;How to enable sparse image in android&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 02:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532562#M84775</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-23T02:04:46Z</dc:date>
    </item>
    <item>
      <title>Re: Increasing the size of initfsram for mfgtool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532563#M84776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jul 2016 02:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Increasing-the-size-of-initfsram-for-mfgtool/m-p/532563#M84776</guid>
      <dc:creator>valentinafernan</dc:creator>
      <dc:date>2016-07-23T02:17:25Z</dc:date>
    </item>
  </channel>
</rss>