<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Incorporating Gstreamer into yocto build in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527623#M84506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SCM-QWKS dev board and I want to include gstreamer into the image build in yocto. I added gstreamer1.0-plugins-imx to my local.conf file and have been able to successfully install it. The only confusion I have now is when I do the following command provided in the Linux User's Guide:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch-1.0 imxv4l2src ! imxv4l2sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imxv4l2src is not recognized. I ran a gst-inspect-1.0 on imxv4l2src and it fails to find it, however, it finds v4l2src just fine. Is this ok or does it have to be imxv4l2src?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Aug 2016 19:39:35 GMT</pubDate>
    <dc:creator>aliismail</dc:creator>
    <dc:date>2016-08-15T19:39:35Z</dc:date>
    <item>
      <title>Incorporating Gstreamer into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527623#M84506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SCM-QWKS dev board and I want to include gstreamer into the image build in yocto. I added gstreamer1.0-plugins-imx to my local.conf file and have been able to successfully install it. The only confusion I have now is when I do the following command provided in the Linux User's Guide:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gst-launch-1.0 imxv4l2src ! imxv4l2sink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imxv4l2src is not recognized. I ran a gst-inspect-1.0 on imxv4l2src and it fails to find it, however, it finds v4l2src just fine. Is this ok or does it have to be imxv4l2src?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Aug 2016 19:39:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527623#M84506</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2016-08-15T19:39:35Z</dc:date>
    </item>
    <item>
      <title>Re: Incorporating Gstreamer into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527624#M84507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ali&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is imxv4l2src, one can try recipes-multimedia described in attached Yocto Guide p.4&lt;/P&gt;&lt;P&gt;or try to build fsl-image-machine-test (Table 1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 00:37:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527624#M84507</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-08-16T00:37:20Z</dc:date>
    </item>
    <item>
      <title>Re: Incorporating Gstreamer into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527625#M84508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Please check if a (MIPI, CSI) camera&amp;nbsp; driver is present in Your system. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 02:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527625#M84508</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-08-16T02:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Incorporating Gstreamer into yocto build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527626#M84509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MIPI CSI camera driver known as what? Can I configure this using menuconfig?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Aug 2016 20:34:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Incorporating-Gstreamer-into-yocto-build/m-p/527626#M84509</guid>
      <dc:creator>aliismail</dc:creator>
      <dc:date>2016-08-16T20:34:45Z</dc:date>
    </item>
  </channel>
</rss>