<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.MX6 ECSPI2 _SCLK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526990#M84472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm new using IMX6 processor and i need a fast solution &lt;BR /&gt;I'm using iMX6_Platform_SDK on a board , i understood the ECSPI module 2 but the output logic level is 1.8 V instead of 3.3 V &lt;BR /&gt;I need help to understand&amp;nbsp; how to make the output voltage 3.3 V ؟&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jul 2016 11:33:36 GMT</pubDate>
    <dc:creator>khaledali</dc:creator>
    <dc:date>2016-07-21T11:33:36Z</dc:date>
    <item>
      <title>I.MX6 ECSPI2 _SCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526990#M84472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm new using IMX6 processor and i need a fast solution &lt;BR /&gt;I'm using iMX6_Platform_SDK on a board , i understood the ECSPI module 2 but the output logic level is 1.8 V instead of 3.3 V &lt;BR /&gt;I need help to understand&amp;nbsp; how to make the output voltage 3.3 V ؟&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jul 2016 11:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526990#M84472</guid>
      <dc:creator>khaledali</dc:creator>
      <dc:date>2016-07-21T11:33:36Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 ECSPI2 _SCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526991#M84473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Khaled&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check voltage of power supply which feeds that pads,&lt;/P&gt;&lt;P&gt;please use processor&amp;nbsp; datasheet, like Table 100. 21 x 21 mm Functional Contact Assignments&lt;/P&gt;&lt;P&gt;i.MX6DQ Datasheet (rev.4, 7/2015)&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6DQCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For i.MX6SL one can also check LVE bit in Pad Control Register (IOMUXC_SW_PAD_CTL_PAD_X_Y)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2016 00:36:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526991#M84473</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-22T00:36:16Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 ECSPI2 _SCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526992#M84474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;first of all thanks to your reply but &lt;/P&gt;&lt;P&gt; i have checked that in my board schematic all supplied voltages needed are connected to 3P3V &lt;/P&gt;&lt;P&gt;and i still have the problem &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Jul 2016 09:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526992#M84474</guid>
      <dc:creator>khaledali</dc:creator>
      <dc:date>2016-07-24T09:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 ECSPI2 _SCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526993#M84475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;also this may be caused by broken pad or board layout error&lt;/P&gt;&lt;P&gt;(some lines, like two outputs connected together).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 00:38:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526993#M84475</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-07-25T00:38:17Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX6 ECSPI2 _SCLK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526994#M84476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you show your dts ecspi2 configuration?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 02:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX6-ECSPI2-SCLK/m-p/526994#M84476</guid>
      <dc:creator>qinghuazhu</dc:creator>
      <dc:date>2016-07-25T02:13:41Z</dc:date>
    </item>
  </channel>
</rss>