<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX233 - LCD issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX233-LCD-issue/m-p/184630#M8443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we are using IMX233 processor for our custom board.&lt;BR /&gt;&lt;BR /&gt;we are facing a problem with the contents being displayed on the LCD (resolution 240x320)&lt;BR /&gt;&lt;BR /&gt;The problem is&amp;nbsp; dots are displayed on icons/multilayered images. &lt;BR /&gt;&lt;BR /&gt;we took a screenshot of the image using remote API &lt;BR /&gt;&lt;BR /&gt;In screenshot we are not able to see the dots (screenshots attached). So we hope that framebuffer &lt;BR /&gt;content is proper.&lt;BR /&gt;&lt;BR /&gt;whether LCD controller which fetches the data from framebuffer does something &lt;BR /&gt;so that dots are visible on screen or PXP ?&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;But we have tried excluding the pxp dll from the image then also the problem remains the same&lt;BR /&gt;&lt;BR /&gt;So is it the LCDIF causing the of the problem ?&lt;BR /&gt;&lt;BR /&gt;The LCDIF settings for our LCD,&lt;BR /&gt;&lt;BR /&gt;using dotclock mode&lt;BR /&gt;Pixel format : RGB565&lt;BR /&gt;databuswidth : 16&lt;BR /&gt;wordlength&amp;nbsp;&amp;nbsp; : 0 ( 16Bpp)&lt;BR /&gt;BYTE_PACKING_FORMAT: 0xF&lt;BR /&gt;&lt;BR /&gt;Please advise us on this issue&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2012 11:07:58 GMT</pubDate>
    <dc:creator>Asha1z</dc:creator>
    <dc:date>2012-08-23T11:07:58Z</dc:date>
    <item>
      <title>IMX233 - LCD issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX233-LCD-issue/m-p/184630#M8443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we are using IMX233 processor for our custom board.&lt;BR /&gt;&lt;BR /&gt;we are facing a problem with the contents being displayed on the LCD (resolution 240x320)&lt;BR /&gt;&lt;BR /&gt;The problem is&amp;nbsp; dots are displayed on icons/multilayered images. &lt;BR /&gt;&lt;BR /&gt;we took a screenshot of the image using remote API &lt;BR /&gt;&lt;BR /&gt;In screenshot we are not able to see the dots (screenshots attached). So we hope that framebuffer &lt;BR /&gt;content is proper.&lt;BR /&gt;&lt;BR /&gt;whether LCD controller which fetches the data from framebuffer does something &lt;BR /&gt;so that dots are visible on screen or PXP ?&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;But we have tried excluding the pxp dll from the image then also the problem remains the same&lt;BR /&gt;&lt;BR /&gt;So is it the LCDIF causing the of the problem ?&lt;BR /&gt;&lt;BR /&gt;The LCDIF settings for our LCD,&lt;BR /&gt;&lt;BR /&gt;using dotclock mode&lt;BR /&gt;Pixel format : RGB565&lt;BR /&gt;databuswidth : 16&lt;BR /&gt;wordlength&amp;nbsp;&amp;nbsp; : 0 ( 16Bpp)&lt;BR /&gt;BYTE_PACKING_FORMAT: 0xF&lt;BR /&gt;&lt;BR /&gt;Please advise us on this issue&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2012 11:07:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX233-LCD-issue/m-p/184630#M8443</guid>
      <dc:creator>Asha1z</dc:creator>
      <dc:date>2012-08-23T11:07:58Z</dc:date>
    </item>
  </channel>
</rss>