<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 framebuffer colour settings in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521523#M84417</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a variscite var-som-mx6 board (with an i.MX6Quad) and a buildroot based software image based on the 3.14.38 Linux kernel with Qt and eglfs/framebuffer (with no directfb or X11 support).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been able to get 2 different types of LVDS screens working, however, The colour temperature of one of the screens is slightly higher than the other resulting in the image looking slightly more blue / washed out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to be able to adjust the colour characteristics to allow for differences in the behaviour of the lcd panels so that the colours appear the same on both screens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the code mentioned here: &lt;A href="https://community.nxp.com/docs/DOC-101053"&gt;i.MX6 CSC setting sample source code&lt;/A&gt; to try and adjust the color temperature however it does not appear to have any effect on the graphics output when displaying a static image using the framebuffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can the CSC be configured to work with RGB graphics output of the framebuffer?&lt;/P&gt;&lt;P&gt;Is there any userspace sample code available that can be used to set the color characteristics?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 14:19:55 GMT</pubDate>
    <dc:creator>wesleyrevens</dc:creator>
    <dc:date>2016-06-15T14:19:55Z</dc:date>
    <item>
      <title>i.MX6 framebuffer colour settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521523#M84417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a variscite var-som-mx6 board (with an i.MX6Quad) and a buildroot based software image based on the 3.14.38 Linux kernel with Qt and eglfs/framebuffer (with no directfb or X11 support).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been able to get 2 different types of LVDS screens working, however, The colour temperature of one of the screens is slightly higher than the other resulting in the image looking slightly more blue / washed out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to be able to adjust the colour characteristics to allow for differences in the behaviour of the lcd panels so that the colours appear the same on both screens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the code mentioned here: &lt;A href="https://community.nxp.com/docs/DOC-101053"&gt;i.MX6 CSC setting sample source code&lt;/A&gt; to try and adjust the color temperature however it does not appear to have any effect on the graphics output when displaying a static image using the framebuffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can the CSC be configured to work with RGB graphics output of the framebuffer?&lt;/P&gt;&lt;P&gt;Is there any userspace sample code available that can be used to set the color characteristics?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 14:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521523#M84417</guid>
      <dc:creator>wesleyrevens</dc:creator>
      <dc:date>2016-06-15T14:19:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 framebuffer colour settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521524#M84418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wesley&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please look at csc usage in sect.7.3.15 Video conversion&lt;/P&gt;&lt;P&gt;attached Linux User Guide. Link below also has some csc examples&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94961"&gt;ipu-examples release notes - v0.1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:42:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521524#M84418</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-16T00:42:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 framebuffer colour settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521525#M84419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Igor, I have had a look at the ipu examples and the csc example converts the pixel formats&lt;/P&gt;&lt;P&gt;of various images images to RGB565. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't been able to find any examples that set the contrast, color, etc of the IPU output&lt;/P&gt;&lt;P&gt;for graphics.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the code mentioned here: &lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-content-finding="Community" data-objectid="101053" data-objecttype="102" href="https://community.nxp.com/docs/DOC-101053"&gt;i.MX6 CSC setting sample source code&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It looks like I need to be using the MXCFB_CSC_UPDATE ioctl command.&lt;/P&gt;&lt;P&gt;However, this command did not appear to do anything to the graphics output when I tested it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 08:29:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521525#M84419</guid>
      <dc:creator>wesleyrevens</dc:creator>
      <dc:date>2016-06-16T08:29:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 framebuffer colour settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521526#M84420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Wesley&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look below at useful answers from our ipu experts&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/373663#comment-373663" title="https://community.nxp.com/message/373663#comment-373663"&gt;https://community.nxp.com/message/373663#comment-373663&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/308426"&gt;iMX6Q display adjustment&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 13:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/521526#M84420</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-16T13:12:43Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 framebuffer colour settings</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/1437606#M188885</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have the exact same behaviour on our VAR-SOM-MX6 connected to an LVDS screen. MXCFB_CSC_UPDATE ioctl command doesn't seem to impact any change on the screen but MXCFB_SET_GAMMA do. How did you resolve this?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 01 Apr 2022 10:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-framebuffer-colour-settings/m-p/1437606#M188885</guid>
      <dc:creator>AntoineP</dc:creator>
      <dc:date>2022-04-01T10:04:00Z</dc:date>
    </item>
  </channel>
</rss>