<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: How to Run a script after leaving sleep mode?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-a-script-after-leaving-sleep-mode/m-p/521055#M84365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi eren&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after resuming, next command after "echo mem &amp;gt; /sys/power/state "&lt;/P&gt;&lt;P&gt;is executed, so one can add necessary command after it as in attached&lt;/P&gt;&lt;P&gt;script example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 07:58:40 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-15T07:58:40Z</dc:date>
    <item>
      <title>How to Run a script after leaving sleep mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-a-script-after-leaving-sleep-mode/m-p/521054#M84364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been using yocto based image on an IMX6 board. I want to run a script when the system wake up from sleep mode? Do you have any suggestion?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 06:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-a-script-after-leaving-sleep-mode/m-p/521054#M84364</guid>
      <dc:creator>erenbasturk</dc:creator>
      <dc:date>2016-06-15T06:48:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to Run a script after leaving sleep mode?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-a-script-after-leaving-sleep-mode/m-p/521055#M84365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi eren&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;after resuming, next command after "echo mem &amp;gt; /sys/power/state "&lt;/P&gt;&lt;P&gt;is executed, so one can add necessary command after it as in attached&lt;/P&gt;&lt;P&gt;script example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 07:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-Run-a-script-after-leaving-sleep-mode/m-p/521055#M84365</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-15T07:58:40Z</dc:date>
    </item>
  </channel>
</rss>