<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520897#M84343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;thank you for your replay. our board runs well before i add patchs to keep logo. i just change lvds clock source from pll2 to pll5 in uboot, it seems well, i need more test. &lt;/P&gt;&lt;P&gt;our screen is 1920x1080, i enable split mode, so which clock source come from for lvds? pll2 or pll5, or both? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 03:00:40 GMT</pubDate>
    <dc:creator>fulinux</dc:creator>
    <dc:date>2016-06-15T03:00:40Z</dc:date>
    <item>
      <title>system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520895#M84341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hardware:imx6q, 4G DDR3, 32G SD;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SoftWare: imx_3.0.101 (base on imx_3.0.35_4.1.0), Qt5.4&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am doing add uboot logo refer to &lt;A href="https://community.nxp.com/docs/DOC-98109"&gt;Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and LVDS)&lt;/A&gt; ,i have compared and modified different patchs all of them, and it seems work well, but it will reboot abnormally when i display a video or copy some files from u disk to board, it reboot with no log, I am very anxious for our products will soon be put into production. we need some advice.&lt;/P&gt;&lt;P&gt;I add attachments here.&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 02:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520895#M84341</guid>
      <dc:creator>fulinux</dc:creator>
      <dc:date>2016-06-15T02:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520896#M84342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if reboot occurs during high intensive memory transfers, as&lt;/P&gt;&lt;P&gt;display a video or copy some files from u disk, this may point to&lt;/P&gt;&lt;P&gt;board noise and memory errors due to that noise.&lt;/P&gt;&lt;P&gt;It may be useful to check power lines with oscilloscope and try to run system with lower frequencies. &lt;/P&gt;&lt;P&gt;Just for test one can try the following experiments to determine if it is a hardware issue.&lt;/P&gt;&lt;P&gt;Hand solder 22uF capacitors directly under center of chip.&amp;nbsp; Solder on top of the 0402 chips.&lt;/P&gt;&lt;P&gt;Have software Increase voltages of ARM_CAP, SOC_CAP, PU_CAP.&lt;/P&gt;&lt;P&gt;Also recommended to rerun ddr test.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/docs/DOC-105652" title="https://community.freescale.com/docs/DOC-105652"&gt;https://community.freescale.com/docs/DOC-105652&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 02:34:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520896#M84342</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-15T02:34:27Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520897#M84343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor,&lt;/P&gt;&lt;P&gt;thank you for your replay. our board runs well before i add patchs to keep logo. i just change lvds clock source from pll2 to pll5 in uboot, it seems well, i need more test. &lt;/P&gt;&lt;P&gt;our screen is 1920x1080, i enable split mode, so which clock source come from for lvds? pll2 or pll5, or both? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 03:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520897#M84343</guid>
      <dc:creator>fulinux</dc:creator>
      <dc:date>2016-06-15T03:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520898#M84344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can try attached patch.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/387331"&gt;imx-ipuv3 2400000.ipu: DC stop timeout after 50 ms&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 05:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520898#M84344</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-15T05:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520899#M84345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi igor,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;i attach my patch file here.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;when i use keep logo from uboot to kernel, power become larger, i have burned two boards, voltage-regulator tube has burned both of them, i think of&amp;nbsp; lvds、di or ipu's clocks are not correct, makes board change the power.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;in uboot:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;we use ipu1 split mode, should we use both di0 and di1?&amp;nbsp; is it correct the modified codes as follows:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;uboot-imx/cpu/arm_cortexa8/mx6/generic.c:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;before:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#ifdef LVDS_CLOCK_SRC_PLL5&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set ldb_di_clk clock source to PLL5 */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = readl(CCM_BASE_ADDR + CLKCTL_CS2CDR);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (di == 0) { &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &amp;amp;= ~(0x7 &amp;lt;&amp;lt; 9);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg |= (0x0 &amp;lt;&amp;lt; 9);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else if (di == 1) { &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &amp;amp;= ~(0x7 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg |= (0x0 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(reg, CCM_BASE_ADDR + CLKCTL_CS2CDR);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#else&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;modified:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#ifdef LVDS_CLOCK_SRC_PLL5&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set ldb_di_clk clock source to PLL5 */&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = readl(CCM_BASE_ADDR + CLKCTL_CS2CDR);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (di == 0) { &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &amp;amp;= ~(0x7 &amp;lt;&amp;lt; 9);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg |= (0x0 &amp;lt;&amp;lt; 9);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;#ifdef LVDS_SPLIT_MODE&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &amp;amp;= ~(0x7 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg |= (0x0 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;#endif&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else if (di == 1) { &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg &amp;amp;= ~(0x7 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg |= (0x0 &amp;lt;&amp;lt; 12); &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writel(reg, CCM_BASE_ADDR + CLKCTL_CS2CDR);&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#else&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;shoud i set di0 and di1's ldb_di_clk clock source to PLL5&amp;nbsp; in split mode.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I am nervous, my boss has been urged me.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jun 2016 09:22:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520899#M84345</guid>
      <dc:creator>fulinux</dc:creator>
      <dc:date>2016-06-21T09:22:10Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520900#M84346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For split mode, only one DI needs be used. For your issue, I think your hardware should check whcih power was increased?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 02:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520900#M84346</guid>
      <dc:creator>qiang_li-mpu_se</dc:creator>
      <dc:date>2016-06-22T02:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: system reboot abnormally when i patch 'upport uboot logo keep from uboot to kernel'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520901#M84347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Thank you for your reply. it is not hardware problem, it happend when i use these patchs. it is the same board. have you see the patch attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jun 2016 01:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/system-reboot-abnormally-when-i-patch-upport-uboot-logo-keep/m-p/520901#M84347</guid>
      <dc:creator>fulinux</dc:creator>
      <dc:date>2016-06-23T01:10:08Z</dc:date>
    </item>
  </channel>
</rss>