<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックVery strange bug</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Very-strange-bug/m-p/184590#M8429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I try to work with imx28evk. I use kernel and rootfs from EVK. Loading kernel via tftp, connecting to rootfs via nfs. And if kernel is loaded EVK resets after SD card insertion.&lt;/P&gt;&lt;P&gt;If SD card is initially inserted EVK works normal but reset occurs after ejection and insertion SD.&lt;/P&gt;&lt;P&gt;Google can't help.&lt;/P&gt;&lt;P&gt;Any Ideas, any assumptions are welcome...&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Aug 2012 09:47:00 GMT</pubDate>
    <dc:creator>AlekseyP_</dc:creator>
    <dc:date>2012-08-30T09:47:00Z</dc:date>
    <item>
      <title>Very strange bug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Very-strange-bug/m-p/184590#M8429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I try to work with imx28evk. I use kernel and rootfs from EVK. Loading kernel via tftp, connecting to rootfs via nfs. And if kernel is loaded EVK resets after SD card insertion.&lt;/P&gt;&lt;P&gt;If SD card is initially inserted EVK works normal but reset occurs after ejection and insertion SD.&lt;/P&gt;&lt;P&gt;Google can't help.&lt;/P&gt;&lt;P&gt;Any Ideas, any assumptions are welcome...&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2012 09:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Very-strange-bug/m-p/184590#M8429</guid>
      <dc:creator>AlekseyP_</dc:creator>
      <dc:date>2012-08-30T09:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: Very strange bug</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Very-strange-bug/m-p/184591#M8430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have never seen this kind of situation, but I can suggest you to start debugging from CARD DETECT routine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In linux kernel linux-2.6.35.3 CARD DETECT is done polling host controller, if you have the possibility to recompile kernel source you can try to bypass this check, to see when reset happens (file drivers/mmc/host/mxs-mmc.c) .&lt;/P&gt;&lt;P&gt;Maybe problems can be generated from&amp;nbsp; power pin of MMC (file arch/arm/mach-mx28/device.c)&lt;/P&gt;&lt;P&gt;Do you see board reset also at u-boot level, if you insert SD in that moment ?&lt;/P&gt;&lt;P&gt;Giuseppe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2012 10:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Very-strange-bug/m-p/184591#M8430</guid>
      <dc:creator>GiuseppePagano</dc:creator>
      <dc:date>2012-08-30T10:32:20Z</dc:date>
    </item>
  </channel>
</rss>