<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Android UI not fix with lcd display in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-UI-not-fix-with-lcd-display/m-p/520159#M84273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aravinth,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The issue should be generated by LCD timing, so you will have to adjust LCD timing according to LCD's datasheet. If you are using LVDS lcd, timing structure is ldb.c( LVDS driver), if your LCD is parallel interface and connected to DISP0 port, timing structure is mxc_lcd.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 03:01:09 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2016-06-16T03:01:09Z</dc:date>
    <item>
      <title>Android UI not fix with lcd display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-UI-not-fix-with-lcd-display/m-p/520158#M84272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I'm working on imx6 android 4.4.3 solo board. LCD resolution is 800x480, Android UI not fulfilled with display. Full UI is coming as little small. Some empty space are there only in left and right of the screen. How to make it full??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Aravinth &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 12:45:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-UI-not-fix-with-lcd-display/m-p/520158#M84272</guid>
      <dc:creator>aravinthkumarja</dc:creator>
      <dc:date>2016-06-14T12:45:20Z</dc:date>
    </item>
    <item>
      <title>Re: Android UI not fix with lcd display</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-UI-not-fix-with-lcd-display/m-p/520159#M84273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aravinth,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The issue should be generated by LCD timing, so you will have to adjust LCD timing according to LCD's datasheet. If you are using LVDS lcd, timing structure is ldb.c( LVDS driver), if your LCD is parallel interface and connected to DISP0 port, timing structure is mxc_lcd.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 03:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-UI-not-fix-with-lcd-display/m-p/520159#M84273</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-06-16T03:01:09Z</dc:date>
    </item>
  </channel>
</rss>