<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MfgTool not running</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-not-running/m-p/519915#M84256</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phill,&lt;/P&gt;&lt;P&gt;Here you are using the &lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;3.10.53_1.1.0-ga&lt;/EM&gt;&lt;/SPAN&gt; version BSP, so you should use the imx-3.10.53-ga-mfg-tools.tar version mfgtool. It will work. Any questions you can contact me.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 02:25:46 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2016-09-29T02:25:46Z</dc:date>
    <item>
      <title>MfgTool not running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-not-running/m-p/519914#M84255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi Guys, &lt;/P&gt;&lt;P&gt;I'm having trouble getting &lt;EM&gt;any&lt;/EM&gt; version of the MfgTool compiling and working using the provided bitbake recipes.&lt;/P&gt;&lt;P&gt;I have a pre-compiled version aquired from Freescale ~2 years ago, using kernel 3.10, that works, but due to new JEDEC standards, I cannot use it any more.&lt;/P&gt;&lt;P&gt;My problem is, the usb enumeration via otg doesn't work. The device appears to boot, and wait for the usb, which never appears.&lt;/P&gt;&lt;P&gt;I have tried, with out any sucess:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;A fresh check out of the MfgTool git and compiling without any modifications - Won't enumerate USB&lt;/LI&gt;&lt;LI&gt;Patching my device trees and kernel patches against v3.10 - After wranging to get booting, won't enumerate USB&lt;/LI&gt;&lt;LI&gt;Building 4.x version of kernel and mfgtool - Won't boot at all&lt;/LI&gt;&lt;LI&gt;Patching my device trees and kernel patches against v4.x - Wont boot at all&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;There appears to be quite a few differences between the 3.10 and 4.x versions. For example, the 4.x version sends g_mass_storage configure commands via uBoot, but 3.10 doesn't send any commands, but my kernel and built against 3.10, is expecting it.&lt;/P&gt;&lt;P&gt;I am very confused. &lt;EM&gt;What am I missing.&lt;/EM&gt; Does NXP have any better documentation avaliable on the mfgtool, how it works, and how to compile it using bitbake?&lt;/P&gt;&lt;P&gt;I am currently using the recipe &lt;EM&gt;fsl-image-mfgtool-initramfs&lt;/EM&gt;, and the documentation &lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;IMXLXYOCTOUG User's Guide Rev L3.10.53_1.1.0-ga, 01/2015, specifically, section 6.2, page 11.&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Your assistance is greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 02:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-not-running/m-p/519914#M84255</guid>
      <dc:creator>phillogden</dc:creator>
      <dc:date>2016-06-14T02:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: MfgTool not running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MfgTool-not-running/m-p/519915#M84256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Phill,&lt;/P&gt;&lt;P&gt;Here you are using the &lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;3.10.53_1.1.0-ga&lt;/EM&gt;&lt;/SPAN&gt; version BSP, so you should use the imx-3.10.53-ga-mfg-tools.tar version mfgtool. It will work. Any questions you can contact me.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 02:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MfgTool-not-running/m-p/519915#M84256</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-09-29T02:25:46Z</dc:date>
    </item>
  </channel>
</rss>