<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Including ssh server in rootfs using yocto configuration  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/519416#M84223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have built imges for IMX6 sabersd board using the following commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga&lt;/P&gt;&lt;P&gt;#repo sync&lt;/P&gt;&lt;P&gt;#source setup-environment build&lt;/P&gt;&lt;P&gt;#bitbake core-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need ssh server on the target, but it is not there in rootfs. &lt;/P&gt;&lt;P&gt;Can you guide, how to enable ssh server to built with "core-image-minimal".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jun 2016 06:53:40 GMT</pubDate>
    <dc:creator>kravik</dc:creator>
    <dc:date>2016-06-13T06:53:40Z</dc:date>
    <item>
      <title>Including ssh server in rootfs using yocto configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/519416#M84223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have built imges for IMX6 sabersd board using the following commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga&lt;/P&gt;&lt;P&gt;#repo sync&lt;/P&gt;&lt;P&gt;#source setup-environment build&lt;/P&gt;&lt;P&gt;#bitbake core-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need ssh server on the target, but it is not there in rootfs. &lt;/P&gt;&lt;P&gt;Can you guide, how to enable ssh server to built with "core-image-minimal".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2016 06:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/519416#M84223</guid>
      <dc:creator>kravik</dc:creator>
      <dc:date>2016-06-13T06:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Including ssh server in rootfs using yocto configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/519417#M84224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; If the needed package (ssh) is not present in the conf/local.conf file - it will not be included in rootfs. &lt;/P&gt;&lt;P&gt;So - just try to add it Yourself ; in particular customers can try to build most full configurations &lt;/P&gt;&lt;P&gt;such "fsl-image-gui" and&amp;nbsp; "fsl-image-qt5".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-94967"&gt;i.MX Yocto Project: How do I add an existing package to an image?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 08:46:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/519417#M84224</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-14T08:46:11Z</dc:date>
    </item>
    <item>
      <title>Re: Including ssh server in rootfs using yocto configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/1402853#M186096</link>
      <description>&lt;P&gt;So the local.conf must have the line&lt;/P&gt;&lt;P&gt;IMAGE_INSTALL_APPEND = " openssh "&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jan 2022 19:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Including-ssh-server-in-rootfs-using-yocto-configuration/m-p/1402853#M186096</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2022-01-20T19:54:59Z</dc:date>
    </item>
  </channel>
</rss>