<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックChanging The Boot console</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Changing-The-Boot-console/m-p/518448#M84154</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI &lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am&amp;nbsp; facing the problem related to serial console . The default console given for our board is at UART1 bu I change it to UART 2.For that I made the below changes in U-boot:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_UART_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2_BASE&lt;/P&gt;&lt;P&gt;#define CONFIG_CONSOLE_DEV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "ttymxc1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also configured the UART in customboard.c file like&lt;/P&gt;&lt;P&gt;iomux_v3_cfg_t const uart2_pads[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_DAT5__UART2_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_DAT4__UART2_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_CMD__UART2_RTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_CLK__UART2_CTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void setup_iomux_uart(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx_iomux_v3_setup_multiple_pads(uart1_pads, ARRAY_SIZE(uart1_pads));&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx_iomux_v3_setup_multiple_pads(uart2_pads, ARRAY_SIZE(uart2_pads));&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;int board_early_init_f(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; setup_iomux_uart();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After doing all these changes when we connect the board its showing garbage value.. But when kernel is loaded then its showing messages on UART2.Please Suggest the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;hrushi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jun 2016 09:32:10 GMT</pubDate>
    <dc:creator>hrushinale</dc:creator>
    <dc:date>2016-06-10T09:32:10Z</dc:date>
    <item>
      <title>Changing The Boot console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-The-Boot-console/m-p/518448#M84154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI &lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am&amp;nbsp; facing the problem related to serial console . The default console given for our board is at UART1 bu I change it to UART 2.For that I made the below changes in U-boot:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_UART_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp; UART2_BASE&lt;/P&gt;&lt;P&gt;#define CONFIG_CONSOLE_DEV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "ttymxc1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also configured the UART in customboard.c file like&lt;/P&gt;&lt;P&gt;iomux_v3_cfg_t const uart2_pads[] = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_DAT5__UART2_TX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_DAT4__UART2_RX_DATA | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_CMD__UART2_RTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MX6_PAD_SD3_CLK__UART2_CTS_B | MUX_PAD_CTRL(UART_PAD_CTRL),&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;static void setup_iomux_uart(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx_iomux_v3_setup_multiple_pads(uart1_pads, ARRAY_SIZE(uart1_pads));&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; imx_iomux_v3_setup_multiple_pads(uart2_pads, ARRAY_SIZE(uart2_pads));&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;int board_early_init_f(void)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; setup_iomux_uart();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After doing all these changes when we connect the board its showing garbage value.. But when kernel is loaded then its showing messages on UART2.Please Suggest the solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;hrushi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 09:32:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-The-Boot-console/m-p/518448#M84154</guid>
      <dc:creator>hrushinale</dc:creator>
      <dc:date>2016-06-10T09:32:10Z</dc:date>
    </item>
    <item>
      <title>Re: Changing The Boot console</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-The-Boot-console/m-p/518449#M84155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hrushi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can debug it using attached Porting Guide&lt;/P&gt;&lt;P&gt;sect.1.4 Debugging, please check uboot/drivers/serial/serial_mxc.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jun 2016 00:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-The-Boot-console/m-p/518449#M84155</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-11T00:59:54Z</dc:date>
    </item>
  </channel>
</rss>