<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Android Emulator on WinCE7 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-Emulator-on-WinCE7/m-p/518373#M84145</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use the i.MX6Q Sabre for our Application based on a WinCE7 OS. Now we would like to know if it's possible to run a Android Emulator on the WinCE7 OS instead of replacing the entire WinCE7 with Android.&lt;/P&gt;&lt;P&gt;Any expiriences with an Emulator and would it support also all the Interfaces of the undelaying WinCE7 OS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would really appreciate any recommendation or instructions how to do it if it's possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jun 2016 13:13:23 GMT</pubDate>
    <dc:creator>wayne7215</dc:creator>
    <dc:date>2016-06-10T13:13:23Z</dc:date>
    <item>
      <title>Android Emulator on WinCE7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Emulator-on-WinCE7/m-p/518373#M84145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use the i.MX6Q Sabre for our Application based on a WinCE7 OS. Now we would like to know if it's possible to run a Android Emulator on the WinCE7 OS instead of replacing the entire WinCE7 with Android.&lt;/P&gt;&lt;P&gt;Any expiriences with an Emulator and would it support also all the Interfaces of the undelaying WinCE7 OS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We would really appreciate any recommendation or instructions how to do it if it's possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 13:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Emulator-on-WinCE7/m-p/518373#M84145</guid>
      <dc:creator>wayne7215</dc:creator>
      <dc:date>2016-06-10T13:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: Android Emulator on WinCE7</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-Emulator-on-WinCE7/m-p/518374#M84146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;There are also available BSPs for Android on i.MX6Q devices (including 4.x, 5.x and 6.x releases) as native operating system; however, emulators are not provided by NXP.&lt;/P&gt;&lt;P&gt;Regarding Windows BSPs support for i.MX, &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-objectid="209412" data-objecttype="3" href="https://community.nxp.com/people/adeneoengineeringteam"&gt;Adeneo Engineering Team&lt;/A&gt; could provide additional details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 02:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-Emulator-on-WinCE7/m-p/518374#M84146</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-06-14T02:05:06Z</dc:date>
    </item>
  </channel>
</rss>