<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can i use EIM for data transfer from FPGA? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518217#M84132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we used EIM in multiplexed mode with an FPGA to do 32-bit transfers and got avg. cycle times of 456ns for a read and 436ns for a write.&amp;nbsp; The actual transfers were taking 156ns for read and 148ns for write and the i.MX6 was inserting about 300ns of delay between cycles (known issue discussed on these forums before).&amp;nbsp; I suspect it would be possible to shave a few cycles off of the read and write times with more work, but this was sufficient for us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jun 2016 15:34:53 GMT</pubDate>
    <dc:creator>andrewdyer</dc:creator>
    <dc:date>2016-06-14T15:34:53Z</dc:date>
    <item>
      <title>Can i use EIM for data transfer from FPGA?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518213#M84128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;---------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Ubuntu 12.04&lt;/P&gt;&lt;P&gt;Kernel 3.14&lt;/P&gt;&lt;P&gt;Yocto system&lt;/P&gt;&lt;P&gt;i.MX6DL sabresd board&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi everyone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to data transfer from FPGA. (16bit data bus)&lt;/P&gt;&lt;P&gt;Can i use EMIF? If i want to use EMIF , what interface can i use?&lt;/P&gt;&lt;P&gt;MMDC? or WEIM?&lt;/P&gt;&lt;P&gt;I think to usually use EIM. right?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN lang="en"&gt;If the wrong decision, please tell us.&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59084i20DB1E0DD78D9BD6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If i use EIM, can i use like below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_9.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59229i7B2314A4B78354A3/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_7.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59214iA919B198F28B1CD9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can i have EIM example code or manual.. or other solution.. for data transfer use EIM from FPGA ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 02:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518213#M84128</guid>
      <dc:creator>hanseunglee</dc:creator>
      <dc:date>2016-06-10T02:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use EIM for data transfer from FPGA?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518214#M84129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hanseung&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, one can use eim interface, for example codes one can&lt;/P&gt;&lt;P&gt;look at attached sdk test and pdf document Chapter 7 Configuring the EIM Driver&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 06:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518214#M84129</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-10T06:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use EIM for data transfer from FPGA?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518215#M84130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your time!&lt;/P&gt;&lt;P&gt;Can i have a question?&lt;/P&gt;&lt;P&gt;Max operating frequency for EIM data transfer is 104Mhz.&lt;/P&gt;&lt;P&gt;if when i use multiplexed address/data mode, is EIM data trasfer rate 52 Mhz?&lt;/P&gt;&lt;P&gt;Do you know that data transfer rate for multiplexed mode?&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 07:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518215#M84130</guid>
      <dc:creator>hanseunglee</dc:creator>
      <dc:date>2016-06-10T07:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use EIM for data transfer from FPGA?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518216#M84131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;clock requirements are the same in multiplexed address/data mode&lt;/P&gt;&lt;P&gt;and timing diagrams can be found in datasheet and RM (EIM chapter).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jun 2016 11:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518216#M84131</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-10T11:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can i use EIM for data transfer from FPGA?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518217#M84132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we used EIM in multiplexed mode with an FPGA to do 32-bit transfers and got avg. cycle times of 456ns for a read and 436ns for a write.&amp;nbsp; The actual transfers were taking 156ns for read and 148ns for write and the i.MX6 was inserting about 300ns of delay between cycles (known issue discussed on these forums before).&amp;nbsp; I suspect it would be possible to shave a few cycles off of the read and write times with more work, but this was sufficient for us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 15:34:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-i-use-EIM-for-data-transfer-from-FPGA/m-p/518217#M84132</guid>
      <dc:creator>andrewdyer</dc:creator>
      <dc:date>2016-06-14T15:34:53Z</dc:date>
    </item>
  </channel>
</rss>