<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Interfacing 12-bit camera with IMX6 EVM  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-12-bit-camera-with-IMX6-EVM/m-p/517015#M84008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My target board based on IMX6Solo is under design. Meanwhile , I need a IMX6 EVM with which I can interface 12 bit parallel camera . Any EVM supports 12- bit camera . I checked few EVM's , I could see 8 bit and 10 bit camera connectors over EVM . Can I do something for the 12-bit Camera ? Any suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jun 2016 13:29:46 GMT</pubDate>
    <dc:creator>adityanagal</dc:creator>
    <dc:date>2016-06-08T13:29:46Z</dc:date>
    <item>
      <title>Interfacing 12-bit camera with IMX6 EVM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-12-bit-camera-with-IMX6-EVM/m-p/517015#M84008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My target board based on IMX6Solo is under design. Meanwhile , I need a IMX6 EVM with which I can interface 12 bit parallel camera . Any EVM supports 12- bit camera . I checked few EVM's , I could see 8 bit and 10 bit camera connectors over EVM . Can I do something for the 12-bit Camera ? Any suggestions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 13:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-12-bit-camera-with-IMX6-EVM/m-p/517015#M84008</guid>
      <dc:creator>adityanagal</dc:creator>
      <dc:date>2016-06-08T13:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: Interfacing 12-bit camera with IMX6 EVM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Interfacing-12-bit-camera-with-IMX6-EVM/m-p/517016#M84009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aditya&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it may be useful to check Table 67. Camera Input Signal Cross Reference,&lt;/P&gt;&lt;P&gt;Format, and Bits Per Cycle i.MX6SDL Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6SDLCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 00:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Interfacing-12-bit-camera-with-IMX6-EVM/m-p/517016#M84009</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-09T00:52:18Z</dc:date>
    </item>
  </channel>
</rss>