<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Why call imx233 is microprocessor?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Why-call-imx233-is-microprocessor/m-p/184429#M8398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tuan Nguyen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically i.MX233 is an application processor, not only a simple microprocessor.&amp;nbsp; It integrates on-chip ram, DRAM controller, and most of the common used interfaces (e.g. I2C, UART, SPI, SD, USB, etc.).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;/P&gt;&lt;P&gt;Raymond&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Oct 2012 03:46:30 GMT</pubDate>
    <dc:creator>RaymondChoi</dc:creator>
    <dc:date>2012-10-16T03:46:30Z</dc:date>
    <item>
      <title>Why call imx233 is microprocessor?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-call-imx233-is-microprocessor/m-p/184428#M8397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have one question about imx233 that I see about MPU vs MCU on some sites define:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MPU = CPU (single chip)&lt;/LI&gt;&lt;LI&gt;MCU = MPU + Peripherals + Memory (single chip).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;So why call imx233 is microprocessor? I see imx233 has Peripherals, Internal RAM...&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2012 07:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-call-imx233-is-microprocessor/m-p/184428#M8397</guid>
      <dc:creator>TuanNguyen</dc:creator>
      <dc:date>2012-08-31T07:23:40Z</dc:date>
    </item>
    <item>
      <title>Re: Why call imx233 is microprocessor?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Why-call-imx233-is-microprocessor/m-p/184429#M8398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tuan Nguyen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically i.MX233 is an application processor, not only a simple microprocessor.&amp;nbsp; It integrates on-chip ram, DRAM controller, and most of the common used interfaces (e.g. I2C, UART, SPI, SD, USB, etc.).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best regards&lt;/P&gt;&lt;P&gt;Raymond&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2012 03:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Why-call-imx233-is-microprocessor/m-p/184429#M8398</guid>
      <dc:creator>RaymondChoi</dc:creator>
      <dc:date>2012-10-16T03:46:30Z</dc:date>
    </item>
  </channel>
</rss>