<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX6SDL GPIO current. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-GPIO-current/m-p/516073#M83906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takashi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. absolute maximum rating of the output current of the GPIO&lt;/P&gt;&lt;P&gt;is not specified by datasheet, yes it is limited by allowable temperature,&lt;/P&gt;&lt;P&gt;which is defined.&lt;/P&gt;&lt;P&gt;2. if you have VOH=2.64V, VOL=0.66V in design, then I believe&lt;/P&gt;&lt;P&gt;this understanding is correct&lt;/P&gt;&lt;P&gt;3. GPIO ports up to 1.3 mA can be used. Regarding "At this time, the VOH output of 3.3 V"&lt;/P&gt;&lt;P&gt;seems datasheet has not such parameter. Please check Table 23. GPIO DC Parameters&lt;/P&gt;&lt;P&gt;i.MX6SDL Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6SDLCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Jun 2016 11:41:20 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-07T11:41:20Z</dc:date>
    <item>
      <title>i.MX6SDL GPIO current.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-GPIO-current/m-p/516072#M83905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community.&lt;/P&gt;&lt;P&gt;Our customer has tree question below.Would please advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1,&lt;/P&gt;&lt;P&gt;The absolute maximum rating of the output current of the GPIO?&lt;/P&gt;&lt;P&gt;Is to destroy and too much current through CMOS transistors?&lt;/P&gt;&lt;P&gt;Q2,&lt;/P&gt;&lt;P&gt;My understanding is correct ? The output current is limited by the VOH/VOL and the DSE.&lt;/P&gt;&lt;P&gt;The examples listed below.&lt;/P&gt;&lt;P&gt;Design examples)OVDD=3.3V and DSE:111 = 20 Ω than (Table36 of IMX6SDLAEC ), VOH=2.64V, VOL=0.66V design.&lt;/P&gt;&lt;P&gt;Ioh = (OVDD-VOH) / 20 Ω = (3.3-2.64) / 20 = 33 mA&lt;/P&gt;&lt;P&gt;IOL = Ω = 0.66 VOL 20 / 20 = 33 mA&lt;/P&gt;&lt;P&gt;Therefore, less than 33 mA &lt;SPAN class="highlighted"&gt;output&lt;/SPAN&gt; current in order to satisfy the VOH/VOL.&lt;/P&gt;&lt;P&gt;Q3,&lt;/P&gt;&lt;P&gt;For our specific use cases.&lt;/P&gt;&lt;P&gt;May be used currently in our system GPIO ports up to 1.3 mA (only one port. Others are used in less than 1 mA).&lt;/P&gt;&lt;P&gt;At this time, the VOH output of 3.3 V. But we would not be able to destroy ?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 02:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-GPIO-current/m-p/516072#M83905</guid>
      <dc:creator>takashitakahash</dc:creator>
      <dc:date>2016-06-07T02:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6SDL GPIO current.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-GPIO-current/m-p/516073#M83906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takashi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. absolute maximum rating of the output current of the GPIO&lt;/P&gt;&lt;P&gt;is not specified by datasheet, yes it is limited by allowable temperature,&lt;/P&gt;&lt;P&gt;which is defined.&lt;/P&gt;&lt;P&gt;2. if you have VOH=2.64V, VOL=0.66V in design, then I believe&lt;/P&gt;&lt;P&gt;this understanding is correct&lt;/P&gt;&lt;P&gt;3. GPIO ports up to 1.3 mA can be used. Regarding "At this time, the VOH output of 3.3 V"&lt;/P&gt;&lt;P&gt;seems datasheet has not such parameter. Please check Table 23. GPIO DC Parameters&lt;/P&gt;&lt;P&gt;i.MX6SDL Datasheet &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fdata_sheet%2FIMX6SDLCEC.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SDLCEC.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 11:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6SDL-GPIO-current/m-p/516073#M83906</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-07T11:41:20Z</dc:date>
    </item>
  </channel>
</rss>