<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX6 UART FIFO overrun error</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515867#M83896</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepika&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try to use flow control (fsl,uart-has-rtscts) as in uart3&lt;/P&gt;&lt;P&gt;&amp;amp;uart3 {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-names = "default";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart3_1&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-assert-gpios = &amp;lt;&amp;amp;max7310_b 4 GPIO_ACTIVE_HIGH&amp;gt;, /* CTS */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;&amp;amp;max7310_c 3 GPIO_ACTIVE_HIGH&amp;gt;; /* RXD and TXD */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,uart-has-rtscts;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* for DTE mode, add below change */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* fsl,dte-mode; */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart3dte_1&amp;gt;; */&lt;/P&gt;&lt;P&gt;}; &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jun 2016 02:03:31 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-08T02:03:31Z</dc:date>
    <item>
      <title>i.MX6 UART FIFO overrun error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515866#M83895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Sabre-AI board running Android M with kernel 3.14.52.&lt;/P&gt;&lt;P&gt;I am trying to interface a GPS device with Android. I am using UART as the communication interface. As soon as the board boots I am getting the following error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;imx-uart 21e8000.serial: Rx FIFO overrun&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the board hangs for sometime. The GPS HAL is not able to communication over UART.&lt;/P&gt;&lt;P&gt;I saw the thread&amp;nbsp; &lt;A href="https://community.nxp.com/thread/382099"&gt;iMX6Quad uart RX Fifo Overrun&lt;/A&gt;&amp;nbsp; but it did not helped me.&lt;/P&gt;&lt;P&gt;Can anyone give me the solution&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 07:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515866#M83895</guid>
      <dc:creator>deepika_t</dc:creator>
      <dc:date>2016-06-07T07:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 UART FIFO overrun error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515867#M83896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Deepika&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please try to use flow control (fsl,uart-has-rtscts) as in uart3&lt;/P&gt;&lt;P&gt;&amp;amp;uart3 {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-names = "default";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart3_1&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pinctrl-assert-gpios = &amp;lt;&amp;amp;max7310_b 4 GPIO_ACTIVE_HIGH&amp;gt;, /* CTS */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;&amp;amp;max7310_c 3 GPIO_ACTIVE_HIGH&amp;gt;; /* RXD and TXD */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,uart-has-rtscts;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* for DTE mode, add below change */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* fsl,dte-mode; */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* pinctrl-0 = &amp;lt;&amp;amp;pinctrl_uart3dte_1&amp;gt;; */&lt;/P&gt;&lt;P&gt;}; &lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6qdl-sabreauto.dtsi?h=imx_4.1.15_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 02:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515867#M83896</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-08T02:03:31Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 UART FIFO overrun error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515868#M83897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;The device is not supporting RTS/CTS. The issue was resolved .It was a connection issue. The lines to which I connected the GPS module was RS232 lines whereas I needed TTL lines.So when I connected my Sabre auto Uart lines to GPS's TTL lines it worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Deepika&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2016 06:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-UART-FIFO-overrun-error/m-p/515868#M83897</guid>
      <dc:creator>deepika_t</dc:creator>
      <dc:date>2016-06-08T06:53:57Z</dc:date>
    </item>
  </channel>
</rss>