<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: wifi device tree in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514544#M83813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong Sun&lt;/P&gt;&lt;P&gt;First, thanks for your quick reply.&lt;/P&gt;&lt;P&gt;I understand that with the device tree you can config GPIOs, IRQ etc.. (and basically&amp;nbsp; and more generally, initialize the pdev pointer which is sent to the probe function with the relevant values)&lt;/P&gt;&lt;P&gt;What I still did not get is how (in this case) the kernel registered the wifi driver if there is no &lt;EM&gt;compatible&lt;/EM&gt; field associated to that driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Jun 2016 07:12:19 GMT</pubDate>
    <dc:creator>sumosumo</dc:creator>
    <dc:date>2016-06-06T07:12:19Z</dc:date>
    <item>
      <title>wifi device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514542#M83811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using wandboard quad and made a minimal filesystem and kernel under yocto framework.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wifi wasn't working with the minimal image , so I manually added the wifi driver (bcm4329-fmac) and the suitable firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my question is: How come wifi is working (there is an interface and i get results on "iw wlan0 scan") without updating the device tree files (I did not encountered any compatible name "&lt;EM&gt;bcm4329-fmac&lt;/EM&gt;") ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jun 2016 21:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514542#M83811</guid>
      <dc:creator>sumosumo</dc:creator>
      <dc:date>2016-06-05T21:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: wifi device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514543#M83812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="230838" data-username="sumosumo" href="https://community.nxp.com/people/sumosumo"&gt;sumo&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; It is very necessary to add wifi to device tree, for example:&lt;/P&gt;&lt;P&gt;(1) Multiplexing SDIO PINs connected to WIFI card&lt;/P&gt;&lt;P&gt;(2) Initializing corresponding data structure of SDIO&lt;/P&gt;&lt;P&gt;(3) Initializing GPIOs for controlling WIFI's power and reset.&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt; Above work must be done in BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Hope above advice can help you !&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 04:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514543#M83812</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-06-06T04:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: wifi device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514544#M83813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong Sun&lt;/P&gt;&lt;P&gt;First, thanks for your quick reply.&lt;/P&gt;&lt;P&gt;I understand that with the device tree you can config GPIOs, IRQ etc.. (and basically&amp;nbsp; and more generally, initialize the pdev pointer which is sent to the probe function with the relevant values)&lt;/P&gt;&lt;P&gt;What I still did not get is how (in this case) the kernel registered the wifi driver if there is no &lt;EM&gt;compatible&lt;/EM&gt; field associated to that driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 07:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514544#M83813</guid>
      <dc:creator>sumosumo</dc:creator>
      <dc:date>2016-06-06T07:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: wifi device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514545#M83814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sumo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;compatible&lt;/EM&gt; field should be in your wifi driver, you can check if there exists a file name of.c, and search the filed.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 04:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514545#M83814</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-06-07T04:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: wifi device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514546#M83815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;shouldn't &lt;EM&gt;compatible&lt;/EM&gt; field be in the driver (of.c in this case) and in the dts file as well ?&lt;/P&gt;&lt;P&gt;Isn't &lt;EM&gt;compatible&lt;/EM&gt; field who makes the binding between device-tree and the driver ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2016 08:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/wifi-device-tree/m-p/514546#M83815</guid>
      <dc:creator>sumosumo</dc:creator>
      <dc:date>2016-06-07T08:12:41Z</dc:date>
    </item>
  </channel>
</rss>