<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: V4L2_MEMORY_USERPTR</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513951#M83772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I think - from performance perspective - it would be better to increase continuous &lt;/P&gt;&lt;P&gt;(DMA) space, say, using "cma=" kernel boot parameter. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:31:18 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2016-06-16T02:31:18Z</dc:date>
    <item>
      <title>V4L2_MEMORY_USERPTR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513948#M83769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are working on the custom IMX6 board. Below are the details.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Processor: iMX6 (Quad)&lt;/P&gt;&lt;P&gt;Interface: MIPI CSI-2&lt;/P&gt;&lt;P&gt;Camera: any MIPI CSI-2 based camera sensor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are passing the buffer from user program to V4l2 using the userptr&lt;/P&gt;&lt;P&gt;For the &lt;STRONG&gt;Linux&lt;/STRONG&gt; iMX6, v4l2 support, &lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;Whether the &lt;STRONG&gt;V4L2_MEMORY_USERPTR&lt;/STRONG&gt; is been supported? &lt;/LI&gt;&lt;LI&gt;If so, which kernel version is tested for this feature? Can you provide the link/reference?&lt;/LI&gt;&lt;LI&gt;Any tested/example code for iMX6 platform?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Thanks,&lt;/P&gt;&lt;P&gt;P.Ashok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 12:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513948#M83769</guid>
      <dc:creator>ashokp</dc:creator>
      <dc:date>2016-06-03T12:26:11Z</dc:date>
    </item>
    <item>
      <title>Re: V4L2_MEMORY_USERPTR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513949#M83770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; the following may be helpful &lt;A href="https://community.nxp.com/thread/359579"&gt;V4L2_MEMORY_USERPTR example for iMX6&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 02:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513949#M83770</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-06T02:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: V4L2_MEMORY_USERPTR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513950#M83771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply. As per the thread, the userptr is only supported for physically contiguous memory. My question is whether iMX6 supports dis-contiguous userptr as well? Meaning, whether iMX6 can receive the streaming data from camera in memory that is discontiguous? If yes, can you point the relevant section in the iMX6 datasheet? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2016 10:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513950#M83771</guid>
      <dc:creator>ashokp</dc:creator>
      <dc:date>2016-06-09T10:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: V4L2_MEMORY_USERPTR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513951#M83772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I think - from performance perspective - it would be better to increase continuous &lt;/P&gt;&lt;P&gt;(DMA) space, say, using "cma=" kernel boot parameter. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/V4L2-MEMORY-USERPTR/m-p/513951#M83772</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2016-06-16T02:31:18Z</dc:date>
    </item>
  </channel>
</rss>