<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: operating range for the MIPI CSI-2 camera</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/operating-range-for-the-MIPI-CSI-2-camera/m-p/513942#M83768</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ashok&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;operating range for the MIPI CSI-2 is only datasheet NVCC_MIPI parameter&lt;/P&gt;&lt;P&gt;in Table 6. Operating Ranges&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;frequency refers to maximum speed of the IPU interface when receives data from MIPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Jun 2016 01:03:38 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-04T01:03:38Z</dc:date>
    <item>
      <title>operating range for the MIPI CSI-2 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/operating-range-for-the-MIPI-CSI-2-camera/m-p/513941#M83767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Is there any operating range for the MIPI CSI-2 camera (minimum/maximum) for receiving the MIPI data from the camera sensor?&lt;/P&gt;&lt;P&gt;Which clock frequency (MHz) does the below information refers to? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reference:&lt;/P&gt;&lt;P&gt;As per the IMX datasheet, the following information is provided in the IPU section&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fast serial interface (MIPI-CSI2):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL style="list-style-type: disc;"&gt;&lt;LI&gt;IPU receives 2 components per cycle from the MIPI-CSI2 interface&lt;/LI&gt;&lt;LI&gt;The maximum speed of the interface is:&lt;/LI&gt;&lt;LI&gt;200Mhz for 4 data lanes configuration&lt;/LI&gt;&lt;LI&gt;250Mhz for 2 data lanes configuration&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The maximum bandwidth of the interface is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL style="list-style-type: disc;"&gt;&lt;LI&gt;200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)&lt;/LI&gt;&lt;LI&gt;187.5Mhz for 3 data lanes configuration (1000Mbps/lane, 375MByte/sec)&lt;/LI&gt;&lt;LI&gt;125Mhz for 2 data lanes configuration (1000Mbps/lane, 250MByte/sec )&lt;/LI&gt;&lt;LI&gt;62.5Mhz for 1 data lane configuration (1000Mbps/lane, 125Mbyte/sec)&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 12:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/operating-range-for-the-MIPI-CSI-2-camera/m-p/513941#M83767</guid>
      <dc:creator>ashokp</dc:creator>
      <dc:date>2016-06-03T12:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: operating range for the MIPI CSI-2 camera</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/operating-range-for-the-MIPI-CSI-2-camera/m-p/513942#M83768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ashok&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;operating range for the MIPI CSI-2 is only datasheet NVCC_MIPI parameter&lt;/P&gt;&lt;P&gt;in Table 6. Operating Ranges&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf"&gt;http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;frequency refers to maximum speed of the IPU interface when receives data from MIPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jun 2016 01:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/operating-range-for-the-MIPI-CSI-2-camera/m-p/513942#M83768</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-04T01:03:38Z</dc:date>
    </item>
  </channel>
</rss>