<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ERR006687 Where does GPIO6 go?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ERR006687-Where-does-GPIO6-go/m-p/513335#M83729</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it can be routed internally using debug signals, as attached&lt;/P&gt;&lt;P&gt;picture shows. For example one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd-enetirq.dts?h=imx_4.1.15_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd-enetirq.dts?h=imx_4.1.15_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59018iFB71D3EBA55D67CF/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jun 2016 02:45:44 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-06-03T02:45:44Z</dc:date>
    <item>
      <title>ERR006687 Where does GPIO6 go?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERR006687-Where-does-GPIO6-go/m-p/513334#M83728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Running: custom board with a NovSOM imx6q&lt;/P&gt;&lt;P&gt;I've read ERR006687, and we feel we should do the hardware mod to work around the erratum in the next board revision.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The description says to mux GPIO6 as ethernet interrupt. My question is what should GPIO6 be connected to? Does&amp;nbsp; it need to be connected to the ethernet phy? Is it already internally connected to the ethernet block in the SoC once muxed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The EE's are confused.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Joshua&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 22:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERR006687-Where-does-GPIO6-go/m-p/513334#M83728</guid>
      <dc:creator>joshuaclayton</dc:creator>
      <dc:date>2016-06-02T22:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: ERR006687 Where does GPIO6 go?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ERR006687-Where-does-GPIO6-go/m-p/513335#M83729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joshua&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it can be routed internally using debug signals, as attached&lt;/P&gt;&lt;P&gt;picture shows. For example one can look at&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd-enetirq.dts?h=imx_4.1.15_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/tree/arch/arm/boot/dts/imx6q-sabresd-enetirq.dts?h=imx_4.1.15_1.0.0_ga"&gt;linux-2.6-imx.git - Freescale i.MX Linux Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59018iFB71D3EBA55D67CF/image-size/large?v=v2&amp;amp;px=999" title="1.jpg" alt="1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 02:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ERR006687-Where-does-GPIO6-go/m-p/513335#M83729</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-06-03T02:45:44Z</dc:date>
    </item>
  </channel>
</rss>