<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VADC &amp; IMX6SX in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/VADC-IMX6SX/m-p/512912#M83673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I'm using imx6sx with fido (kernel 3.14.28)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; when I launch:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;EM&gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0 &lt;BR /&gt; &lt;BR /&gt; &lt;/EM&gt;I have a&amp;nbsp; lots of &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86900000 != 86b00000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86b00000 != 87300000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86d00000 != 86f00000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86f00000 != 87100000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 87100000 != 86700000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86700000 != 86900000&lt;/P&gt;&lt;P&gt; ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; and the image (on the video0) is wrong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If I interrupt the gst-launch the memory is corrupted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; -sh: /usr/bin/free: Accessing a corrupted shared library&lt;/P&gt;&lt;P&gt; -sh: symbol lookup error: /lib/libc.so.6: undefined symbol: __tls_get_addr, version GLIBC_2.4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Any help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 May 2016 16:14:56 GMT</pubDate>
    <dc:creator>mirkoardinghi1</dc:creator>
    <dc:date>2016-05-10T16:14:56Z</dc:date>
    <item>
      <title>VADC &amp; IMX6SX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VADC-IMX6SX/m-p/512912#M83673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I'm using imx6sx with fido (kernel 3.14.28)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; when I launch:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;EM&gt;gst-launch-1.0 imxv4l2src device=/dev/video1 ! imxv4l2sink device=/dev/video0 &lt;BR /&gt; &lt;BR /&gt; &lt;/EM&gt;I have a&amp;nbsp; lots of &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86900000 != 86b00000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86b00000 != 87300000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86d00000 != 86f00000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86f00000 != 87100000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 87100000 != 86700000&lt;/P&gt;&lt;P&gt; mx6s-csi 221c000.csi: 86700000 != 86900000&lt;/P&gt;&lt;P&gt; ....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; and the image (on the video0) is wrong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If I interrupt the gst-launch the memory is corrupted&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; -sh: /usr/bin/free: Accessing a corrupted shared library&lt;/P&gt;&lt;P&gt; -sh: symbol lookup error: /lib/libc.so.6: undefined symbol: __tls_get_addr, version GLIBC_2.4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; Any help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2016 16:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VADC-IMX6SX/m-p/512912#M83673</guid>
      <dc:creator>mirkoardinghi1</dc:creator>
      <dc:date>2016-05-10T16:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: VADC &amp; IMX6SX</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/VADC-IMX6SX/m-p/512913#M83674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mirko,&lt;/P&gt;&lt;P&gt;It is recommended trying with the most recent Linux release. You could take a look at L4.1.15_1.0.0_iMX6SX BSP.&lt;/P&gt;&lt;P&gt;Additionally, the following thread could provide useful information:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381386"&gt;iMX6SX: VADC: force video standard&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 May 2016 23:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/VADC-IMX6SX/m-p/512913#M83674</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2016-05-16T23:48:31Z</dc:date>
    </item>
  </channel>
</rss>