<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Sluggish Performance on imx6S with Android 5.1.1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Sluggish-Performance-on-imx6S-with-Android-5-1-1/m-p/512788#M83661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a custom board with imx6 solo and are experiencing sluggish general performance (android GUI lags etc).&amp;nbsp; A simple test is to plug in a USB mouse and move it around on the android home desktop and it'll cap the CPU neat 100% usage without doing anything else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For reference:&lt;/P&gt;&lt;P&gt;- This custom board runs Android 4.4.3 without issue.&lt;/P&gt;&lt;P&gt;- The new Android 5.1.1 runs on the sabre sd board (with quad core) without issue&lt;/P&gt;&lt;P&gt;- Disabling 3xcores on the sabre sd board, and limiting the single core to 396MHz significantly outperforms our Solo board @ 800MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've done some benchmarking using the 'antutu' benchmark.&amp;nbsp; It looks like it's the 'runtime' benchmark component that is the culprit.&amp;nbsp; RAM/GPU/IO speeds are comparable between the boards.&amp;nbsp; We've also run some other benchmarks where simple tests such as zip/unzip/AES etc are orders of magnitude worse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect we've missed something obvious (or something has changed between the 4.4.3 builds and 5.1.1).&amp;nbsp; The device tree has been rebuilt, and uboot is the same on the 4.4.3 and 5.1.1 build tests.&amp;nbsp; Any ideas on how we can narrow down this down or any further tests that can be performed?&amp;nbsp; Platform is stable otherwise. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 06:34:28 GMT</pubDate>
    <dc:creator>mark_m</dc:creator>
    <dc:date>2016-03-30T06:34:28Z</dc:date>
    <item>
      <title>Sluggish Performance on imx6S with Android 5.1.1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Sluggish-Performance-on-imx6S-with-Android-5-1-1/m-p/512788#M83661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a custom board with imx6 solo and are experiencing sluggish general performance (android GUI lags etc).&amp;nbsp; A simple test is to plug in a USB mouse and move it around on the android home desktop and it'll cap the CPU neat 100% usage without doing anything else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For reference:&lt;/P&gt;&lt;P&gt;- This custom board runs Android 4.4.3 without issue.&lt;/P&gt;&lt;P&gt;- The new Android 5.1.1 runs on the sabre sd board (with quad core) without issue&lt;/P&gt;&lt;P&gt;- Disabling 3xcores on the sabre sd board, and limiting the single core to 396MHz significantly outperforms our Solo board @ 800MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've done some benchmarking using the 'antutu' benchmark.&amp;nbsp; It looks like it's the 'runtime' benchmark component that is the culprit.&amp;nbsp; RAM/GPU/IO speeds are comparable between the boards.&amp;nbsp; We've also run some other benchmarks where simple tests such as zip/unzip/AES etc are orders of magnitude worse.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect we've missed something obvious (or something has changed between the 4.4.3 builds and 5.1.1).&amp;nbsp; The device tree has been rebuilt, and uboot is the same on the 4.4.3 and 5.1.1 build tests.&amp;nbsp; Any ideas on how we can narrow down this down or any further tests that can be performed?&amp;nbsp; Platform is stable otherwise. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 06:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Sluggish-Performance-on-imx6S-with-Android-5-1-1/m-p/512788#M83661</guid>
      <dc:creator>mark_m</dc:creator>
      <dc:date>2016-03-30T06:34:28Z</dc:date>
    </item>
  </channel>
</rss>