<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AA104SH02-T1 display problem with imx257 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512695#M83636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;another reason may be i.MX25 erratum "TLSbo95476 LCDC: LSCLK is missing",&lt;/P&gt;&lt;P&gt;that is:&lt;/P&gt;&lt;P&gt;LVDS requires a serialized stream where the RGB pixel data and LCD timing &lt;/P&gt;&lt;P&gt;are encapsulated. Using an external circuit which PLL base would be the PIXCLK, &lt;/P&gt;&lt;P&gt;the RGB data and timing could be serialized. This works for 12bpp and 16bpp but &lt;/P&gt;&lt;P&gt;unfortunately for 2bpp, 4bpp, 8bpp, 18bpp and 24bpp, LSCLK skips one cycle &lt;/P&gt;&lt;P&gt;every DE rising, every VSYNC rising and every VSYNC falling. These glitches do &lt;/P&gt;&lt;P&gt;not affect TFT panels because during this time all signals are ignored for the &lt;/P&gt;&lt;P&gt;TFT LCD panel but causes LVDS serialization to fail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Apr 2016 10:54:48 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-04-19T10:54:48Z</dc:date>
    <item>
      <title>AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512691#M83632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello :&lt;/P&gt;&lt;P&gt;I am using the follow way connect to my lcd with lvds signal .I use th 16bpp mode ,&lt;/P&gt;&lt;P&gt;LCDC_LD0 which is&amp;nbsp;&amp;nbsp; R0 and&amp;nbsp; LCDC_LD12 is B0. They&amp;nbsp; should not active at all.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="lvds_conn.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32438iA3BF331DEC1CAAFC/image-size/large?v=v2&amp;amp;px=999" role="button" title="lvds_conn.jpg" alt="lvds_conn.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="lcd.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32897iA738C5697E095265/image-size/large?v=v2&amp;amp;px=999" role="button" title="lcd.JPG" alt="lcd.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It is strange that the blue color is not working fine. I using qt to test it &lt;/P&gt;&lt;P&gt;When I set the RGB color to blue most in qt&amp;nbsp; that is (0,0,255) ,it is B1 to B5 are all 1.&lt;/P&gt;&lt;P&gt;The screen looks like crash,nothing is display on the creen,but when I set blue to lower,&lt;/P&gt;&lt;P&gt;the value is below (0,0.180) then it behave normal.&lt;/P&gt;&lt;P&gt;However,the RED and green behave normal.&lt;/P&gt;&lt;P&gt;The AA104SH02 lcd only use the OE signal of the cpu.&lt;/P&gt;&lt;P&gt;It seems that the blue have influence to OE signal of&amp;nbsp; LCD.&lt;/P&gt;&lt;P&gt;I have look the THC63LVDM83D manual ,it should match the requirment of the LCD.&lt;/P&gt;&lt;P&gt;I test it in uboot and linux ,it behave the same.&lt;/P&gt;&lt;P&gt;Can any one&amp;nbsp; have some idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 07:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512691#M83632</guid>
      <dc:creator>wangliang</dc:creator>
      <dc:date>2016-04-19T07:07:38Z</dc:date>
    </item>
    <item>
      <title>Re: AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512692#M83633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi wang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reason may be SCLK jitter, as i.MX25 was not designed for lvds&lt;/P&gt;&lt;P&gt;converters usage. One can try to use appropriate clock from&lt;/P&gt;&lt;P&gt;CKO pin, using MCR register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 07:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512692#M83633</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-19T07:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512693#M83634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear igor:&lt;/P&gt;&lt;P&gt;The SCLK is LCDC_LSCLK of imx257 ,I measure on the scope it is 40MHz and it is stable.&lt;/P&gt;&lt;P&gt;I set the pcd to value 2,and set parent clk of lcdc_lsclk to upll which is 120MHz,so it is LCDC_LSCLK is 40MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 07:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512693#M83634</guid>
      <dc:creator>wangliang</dc:creator>
      <dc:date>2016-04-19T07:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512694#M83635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Dear igor:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I have try the CLKO as the clock in of the LVDS converter ,i measure the&amp;nbsp; CLKO on the scope the frequency is 40MHz,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;some time it is jump to 39.85MHz .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;The result is same ,the color is wrong.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I am sure&amp;nbsp; that the route of the board is correct. No signal connection wrong on PCB ,and no cable is wrong.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;wangl&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 10:42:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512694#M83635</guid>
      <dc:creator>wangliang</dc:creator>
      <dc:date>2016-04-19T10:42:14Z</dc:date>
    </item>
    <item>
      <title>Re: AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512695#M83636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;another reason may be i.MX25 erratum "TLSbo95476 LCDC: LSCLK is missing",&lt;/P&gt;&lt;P&gt;that is:&lt;/P&gt;&lt;P&gt;LVDS requires a serialized stream where the RGB pixel data and LCD timing &lt;/P&gt;&lt;P&gt;are encapsulated. Using an external circuit which PLL base would be the PIXCLK, &lt;/P&gt;&lt;P&gt;the RGB data and timing could be serialized. This works for 12bpp and 16bpp but &lt;/P&gt;&lt;P&gt;unfortunately for 2bpp, 4bpp, 8bpp, 18bpp and 24bpp, LSCLK skips one cycle &lt;/P&gt;&lt;P&gt;every DE rising, every VSYNC rising and every VSYNC falling. These glitches do &lt;/P&gt;&lt;P&gt;not affect TFT panels because during this time all signals are ignored for the &lt;/P&gt;&lt;P&gt;TFT LCD panel but causes LVDS serialization to fail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 10:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512695#M83636</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-04-19T10:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: AA104SH02-T1 display problem with imx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512696#M83637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi igor:&lt;/P&gt;&lt;P&gt;I am using 16bpp mode,so it should no influence.&lt;/P&gt;&lt;P&gt;And I have changed the PIXCLK to CLKO .But problem still exist.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2016 02:02:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/AA104SH02-T1-display-problem-with-imx257/m-p/512696#M83637</guid>
      <dc:creator>wangliang</dc:creator>
      <dc:date>2016-04-20T02:02:48Z</dc:date>
    </item>
  </channel>
</rss>