<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Command line issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Command-line-issue/m-p/512606#M83606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bordon，&lt;/P&gt;&lt;P&gt;Yes, You can change the command line in the u-boot command in the u-boot source code. When the u-boot boot up, you do not need to configure the u-boot command again. Here you can go to the u-boot source code, the command setting is in the /u-boot-ijmx/2015.04-r0/git/include/configs/mx6sabresd.h. You can try. I have tried the setting in the L3.0.35_4.1.0_130816_source version BSP, it works well. About the new BSP, you can try. And then you can tell me the result. And I will also try it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2016 03:34:14 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2016-09-29T03:34:14Z</dc:date>
    <item>
      <title>Command line issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Command-line-issue/m-p/512605#M83605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I download the IMX6_L5.1_2.1.0 version for Android.&lt;/P&gt;&lt;P&gt;After the system boot-up, I saw the kernel command line is&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.serialno=1202a1d4d82c37a0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I change the command line from the bootloader or kernel from the source code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Bordon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 May 2016 02:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Command-line-issue/m-p/512605#M83605</guid>
      <dc:creator>bordonkuo</dc:creator>
      <dc:date>2016-05-11T02:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Command line issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Command-line-issue/m-p/512606#M83606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bordon，&lt;/P&gt;&lt;P&gt;Yes, You can change the command line in the u-boot command in the u-boot source code. When the u-boot boot up, you do not need to configure the u-boot command again. Here you can go to the u-boot source code, the command setting is in the /u-boot-ijmx/2015.04-r0/git/include/configs/mx6sabresd.h. You can try. I have tried the setting in the L3.0.35_4.1.0_130816_source version BSP, it works well. About the new BSP, you can try. And then you can tell me the result. And I will also try it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Rita&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Mark Correct&amp;nbsp; button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2016 03:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Command-line-issue/m-p/512606#M83606</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2016-09-29T03:34:14Z</dc:date>
    </item>
  </channel>
</rss>