<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question, i.MX6Solo parallel camera input port in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512320#M83580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer wants to use Maxim/MAX9272, Deserializer, for camera input of i.MX6Solo.&lt;/P&gt;&lt;P&gt;As for the parallel output from MAX9272, a spread spectrum(1%) is added.&lt;/P&gt;&lt;P&gt;Can i.MX6SL receive the parallel data from MX9271 correctly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Mar 2016 07:24:28 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2016-03-30T07:24:28Z</dc:date>
    <item>
      <title>Question, i.MX6Solo parallel camera input port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512320#M83580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer wants to use Maxim/MAX9272, Deserializer, for camera input of i.MX6Solo.&lt;/P&gt;&lt;P&gt;As for the parallel output from MAX9272, a spread spectrum(1%) is added.&lt;/P&gt;&lt;P&gt;Can i.MX6SL receive the parallel data from MX9271 correctly?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 07:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512320#M83580</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-03-30T07:24:28Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Solo parallel camera input port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512321#M83581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is possible to use the MAX9272 on the parallel CSI input port of i.MX6SL with 1% spread spectrum on pixel clock/output. Also, please note that the CSI port of i.MX6SL is maximum 16-bit wide, so, the corresponding data format should be selected on the link/deserializer side.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 10:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512321#M83581</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-03-31T10:42:29Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Solo parallel camera input port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512322#M83582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Artur,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;Can i understand that there is no special setting for i.MX6 to receive 1% SS signal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 04:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512322#M83582</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2016-04-04T04:38:27Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Solo parallel camera input port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512323#M83583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, no special settings are required for i.MX6 to get the 1% spread spectrum CSI input. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Apr 2016 07:42:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Solo-parallel-camera-input-port/m-p/512323#M83583</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-04-04T07:42:06Z</dc:date>
    </item>
  </channel>
</rss>