<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx6ul evk - Arduino pin usage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512191#M83519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi giuliano&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on EVK this line D7 is disconnected (R1731 is DNP) from processor&lt;/P&gt;&lt;P&gt;pad SD1_DATA1. SD1_DATA1 is GPIO2_IO19 according to p.183&lt;/P&gt;&lt;P&gt;Chapter 4 External Signals and Pin Multiplexing i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6ULRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;GPIO example with linux is provided on:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317876"&gt;Any examples on how to modify the .dts (device tree) source for custom hardware?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Mar 2016 01:37:50 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2016-03-09T01:37:50Z</dc:date>
    <item>
      <title>imx6ul evk - Arduino pin usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512190#M83518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm having some trouble using the digital gpios of the arduino header. I'm using the "imx6ul-14x14-evk-btwifi" device tree, but I can't set nor read any gpio.&lt;/P&gt;&lt;P&gt;I've found in the "i.MX 6UltraLite EVK Board Hardware User’s Guide"&amp;nbsp; that array:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58659i6488D52FECF7A441/image-size/large?v=v2&amp;amp;px=999" title="Screenshot from 2016-03-08 15_22_25.png" alt="Screenshot from 2016-03-08 15_22_25.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I assumed that, for example, if I want to set the pin D7 high, I'll have to work with the gpio 32*3 + 7 = 103 in Linux. I got no error when I export the pin, write its direction etc... but nothing is happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Must I change something in the device tree? I must say I'm not really used to work with these beasts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 14:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512190#M83518</guid>
      <dc:creator>giulianofranche</dc:creator>
      <dc:date>2016-03-08T14:27:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul evk - Arduino pin usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512191#M83519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi giuliano&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on EVK this line D7 is disconnected (R1731 is DNP) from processor&lt;/P&gt;&lt;P&gt;pad SD1_DATA1. SD1_DATA1 is GPIO2_IO19 according to p.183&lt;/P&gt;&lt;P&gt;Chapter 4 External Signals and Pin Multiplexing i.MX6UL Reference Manual &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.freescale.com%2Ffiles%2F32bit%2Fdoc%2Fref_manual%2FIMX6ULRM.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6ULRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;GPIO example with linux is provided on:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317876"&gt;Any examples on how to modify the .dts (device tree) source for custom hardware?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 01:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512191#M83519</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-09T01:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul evk - Arduino pin usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512192#M83520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer Igor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think there is something I still don't understand. How did you link the D7 pin in the hardware user guide, the R1731, and SD1_DATA1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I must be blind ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your patience&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 06:07:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512192#M83520</guid>
      <dc:creator>giulianofranche</dc:creator>
      <dc:date>2016-03-09T06:07:08Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ul evk - Arduino pin usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512193#M83521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;one can look at EVK schematic SPF-28616_C.pdf&amp;nbsp; p.12&lt;/P&gt;&lt;P&gt;Schematics (1)&lt;/P&gt;&lt;P&gt;MCIMX6UL-EVK_DESIGNFILES&lt;/P&gt;&lt;P&gt;Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 0) &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsensors%2Fgyroscopes%2Fi.mx6ultralite-evaluation-kit%3AMCIMX6UL-EVK%3Ffpsp%3D1%26tab%3DDesign_Tools_Tab" rel="nofollow" target="_blank"&gt;http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;~igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 07:35:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ul-evk-Arduino-pin-usage/m-p/512193#M83521</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-09T07:35:56Z</dc:date>
    </item>
  </channel>
</rss>