<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Wandboard DL SD card readiness in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-DL-SD-card-readiness/m-p/512028#M83495</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am not able to find procedure for flashing the Android 5.0.1 build into the SD card for Wandboard DL. I am able to successfully compile the repository and the images are generated. It would be great if I could be pointed to few documentation regarding the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried flashing using the fsl script where it expects "u-boot.imx" file which is not generated as part of compilation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lyf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 May 2016 11:34:09 GMT</pubDate>
    <dc:creator>lyfsci</dc:creator>
    <dc:date>2016-05-10T11:34:09Z</dc:date>
    <item>
      <title>Wandboard DL SD card readiness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-DL-SD-card-readiness/m-p/512028#M83495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am not able to find procedure for flashing the Android 5.0.1 build into the SD card for Wandboard DL. I am able to successfully compile the repository and the images are generated. It would be great if I could be pointed to few documentation regarding the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried flashing using the fsl script where it expects "u-boot.imx" file which is not generated as part of compilation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lyf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 May 2016 11:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wandboard-DL-SD-card-readiness/m-p/512028#M83495</guid>
      <dc:creator>lyfsci</dc:creator>
      <dc:date>2016-05-10T11:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: Wandboard DL SD card readiness</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wandboard-DL-SD-card-readiness/m-p/512029#M83496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Refer to attached Quick Start Guide document (starting from the Page 2). This document is also available on the Wandboard web site:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fwww.wandboard.org%2Findex.php%2Fdownloads" rel="nofollow" target="_blank"&gt;http://www.wandboard.org/index.php/downloads&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 10:28:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wandboard-DL-SD-card-readiness/m-p/512029#M83496</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-05-12T10:28:44Z</dc:date>
    </item>
  </channel>
</rss>