<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MPlayer with poor performances</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184221#M8341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;because of vpu,the mplayer's decodes is softdecode ,you shoud add the vpu unit to the mplayer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2012 05:44:34 GMT</pubDate>
    <dc:creator>haitao</dc:creator>
    <dc:date>2012-09-27T05:44:34Z</dc:date>
    <item>
      <title>MPlayer with poor performances</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184219#M8339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have built the mplayer included into LTIB and ran it on my i.MX51 EVK board. I tried it with an avi file and I got very poor performances. Is that normal?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here some furhter details on my MPlayer:&lt;/P&gt;&lt;P&gt;root@freescale /usr/local/Trolltech/demos/embedded/fluidlauncher$ mplayer --vers&lt;BR /&gt;ion&lt;BR /&gt;MPlayer 1.0rc2-4.4.4 (C) 2000-2007 MPlayer Team&lt;BR /&gt;Unknown option on the command line: --version&lt;BR /&gt;Error parsing option on the command line: --version&lt;BR /&gt;root@freescale /usr/local/Trolltech/demos/embedded/fluidlauncher$ mplayer -v&lt;BR /&gt;MPlayer 1.0rc2-4.4.4 (C) 2000-2007 MPlayer Team&lt;BR /&gt;get_path('codecs.conf') -&amp;gt; '/root/.mplayer/codecs.conf'&lt;BR /&gt;Reading /root/.mplayer/codecs.conf: Can't open '/root/.mplayer/codecs.conf': No such file or directory&lt;BR /&gt;Reading /usr/local/etc/mplayer/codecs.conf: Can't open '/usr/local/etc/mplayer/codecs.conf': No such file or directory&lt;BR /&gt;Using built-in default codecs.conf.&lt;BR /&gt;Usage:&amp;nbsp;&amp;nbsp; mplayer [options] [url|path/]filename&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Packages added in LTIB:&lt;/P&gt;&lt;P&gt;amd-gpu-bin-mx51&lt;/P&gt;&lt;P&gt;libz160-bin&lt;/P&gt;&lt;P&gt;ffmpeg&lt;/P&gt;&lt;P&gt;DirectFB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can I do to tune the mplayer tool?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Nov 2011 00:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184219#M8339</guid>
      <dc:creator>bonil</dc:creator>
      <dc:date>2011-11-06T00:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: MPlayer with poor performances</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184220#M8340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I could answer to my question by myself.. now I'm using gplay that is much better!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Nov 2011 18:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184220#M8340</guid>
      <dc:creator>bonil</dc:creator>
      <dc:date>2011-11-21T18:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: MPlayer with poor performances</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184221#M8341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;because of vpu,the mplayer's decodes is softdecode ,you shoud add the vpu unit to the mplayer!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 05:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MPlayer-with-poor-performances/m-p/184221#M8341</guid>
      <dc:creator>haitao</dc:creator>
      <dc:date>2012-09-27T05:44:34Z</dc:date>
    </item>
  </channel>
</rss>