<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue with Nitrogten6x_MAX DVI Output in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-Nitrogten6x-MAX-DVI-Output/m-p/511334#M83366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having an issue with the output of the Nitrogten6x_MAX board, specifically using a HDMI to DVI cable.&lt;/P&gt;&lt;P&gt;I worked through a few issues in the kernel and have made some headway, but I am stuck with one last problem.&amp;nbsp; Every once in a while, and sometimes very consistently, the screen will output red or blue vertical lines overlaying the desktop.&amp;nbsp; This does not happen with every output device I plug into it, but on some it is very consistent.&amp;nbsp; The lines are usually a few pixels thick and sparkle on the right side (meaning the pixels are solid on the left but random on the right of the lines).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I unplug the cable and plug it back in, everything is fine, until I boot up again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am hooking up to some DVI output boards which are rated to take 1024x768 @ 60hz and work great on a windows PC.&amp;nbsp; I have rewritten part of the kernel to specifically set itself to 1024x768 @ 60hz if that mode is identified in the EDID chip and 1920x1080 @ 60hz is not identified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried changing the frequency down to 30hz and back up to 50, 55, 57, 59, 59.94, 60, and 61.&amp;nbsp; No real change.&amp;nbsp; I notice there is a difference when using a single-link and a double-link cable, but both will produce the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone dealt with this in the past or does anyone have any input on how to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Mar 2016 18:53:28 GMT</pubDate>
    <dc:creator>stevenlopes</dc:creator>
    <dc:date>2016-03-29T18:53:28Z</dc:date>
    <item>
      <title>Issue with Nitrogten6x_MAX DVI Output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-Nitrogten6x-MAX-DVI-Output/m-p/511334#M83366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having an issue with the output of the Nitrogten6x_MAX board, specifically using a HDMI to DVI cable.&lt;/P&gt;&lt;P&gt;I worked through a few issues in the kernel and have made some headway, but I am stuck with one last problem.&amp;nbsp; Every once in a while, and sometimes very consistently, the screen will output red or blue vertical lines overlaying the desktop.&amp;nbsp; This does not happen with every output device I plug into it, but on some it is very consistent.&amp;nbsp; The lines are usually a few pixels thick and sparkle on the right side (meaning the pixels are solid on the left but random on the right of the lines).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I unplug the cable and plug it back in, everything is fine, until I boot up again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am hooking up to some DVI output boards which are rated to take 1024x768 @ 60hz and work great on a windows PC.&amp;nbsp; I have rewritten part of the kernel to specifically set itself to 1024x768 @ 60hz if that mode is identified in the EDID chip and 1920x1080 @ 60hz is not identified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried changing the frequency down to 30hz and back up to 50, 55, 57, 59, 59.94, 60, and 61.&amp;nbsp; No real change.&amp;nbsp; I notice there is a difference when using a single-link and a double-link cable, but both will produce the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone dealt with this in the past or does anyone have any input on how to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Mar 2016 18:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-Nitrogten6x-MAX-DVI-Output/m-p/511334#M83366</guid>
      <dc:creator>stevenlopes</dc:creator>
      <dc:date>2016-03-29T18:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with Nitrogten6x_MAX DVI Output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-with-Nitrogten6x-MAX-DVI-Output/m-p/511335#M83367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you have hdmi enabled in u-boot one can try to disable HDMI in u-boot and&lt;/P&gt;&lt;P&gt;let Linux initialize it:&lt;/P&gt;&lt;P&gt;&lt;A href="https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703" title="https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703"&gt;https://bugzilla.yoctoproject.org/show_bug.cgi?id=6703&lt;/A&gt; &lt;/P&gt;&lt;P&gt;DVI on boundary devices is decribed on:&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/dvi-support-on-i-mx6-boards" title="http://boundarydevices.com/dvi-support-on-i-mx6-boards"&gt;http://boundarydevices.com/dvi-support-on-i-mx6-boards&lt;/A&gt; &lt;/P&gt;&lt;P&gt;Also preferable option is to use true HDMI monitor, in addition to DVI&lt;/P&gt;&lt;P&gt;signals HDMI provides control lines (I2C) for configuring, audio, hot plugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 01:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-with-Nitrogten6x-MAX-DVI-Output/m-p/511335#M83367</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2016-03-30T01:28:04Z</dc:date>
    </item>
  </channel>
</rss>