<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic how to setup GPMI NAND timing in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183948#M8306</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Linux gpmi nand driver for imx28evk, I can not find the code to setup timing parameters into hardware registers. For example, in gpmi-nfc-hal-v1.c, the funtion&amp;nbsp;set_timing(...) doesn't really write nfc's hardware registers, the function is as follows:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * set_timing() - Configures the NFC timing.&lt;BR /&gt; *&lt;BR /&gt; * @this: Per-device data.&lt;BR /&gt; * @timing: The timing of interest.&lt;BR /&gt; */&lt;BR /&gt;static int set_timing(struct gpmi_nfc_data *this,&lt;BR /&gt; const struct gpmi_nfc_timing *timing)&lt;BR /&gt;{&lt;BR /&gt; struct nfc_hal *nfc = this-&amp;gt;nfc;&lt;/P&gt;&lt;P&gt;/* Accept the new timing. */&lt;/P&gt;&lt;P&gt;nfc-&amp;gt;timing = *timing;&lt;/P&gt;&lt;P&gt;/* Return success. */&lt;/P&gt;&lt;P&gt;return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some helps are needed for me to figure this problem out. Thanks very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;P&gt;Emtronix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Aug 2012 08:54:14 GMT</pubDate>
    <dc:creator>x10</dc:creator>
    <dc:date>2012-08-27T08:54:14Z</dc:date>
    <item>
      <title>how to setup GPMI NAND timing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183948#M8306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Linux gpmi nand driver for imx28evk, I can not find the code to setup timing parameters into hardware registers. For example, in gpmi-nfc-hal-v1.c, the funtion&amp;nbsp;set_timing(...) doesn't really write nfc's hardware registers, the function is as follows:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/**&lt;BR /&gt; * set_timing() - Configures the NFC timing.&lt;BR /&gt; *&lt;BR /&gt; * @this: Per-device data.&lt;BR /&gt; * @timing: The timing of interest.&lt;BR /&gt; */&lt;BR /&gt;static int set_timing(struct gpmi_nfc_data *this,&lt;BR /&gt; const struct gpmi_nfc_timing *timing)&lt;BR /&gt;{&lt;BR /&gt; struct nfc_hal *nfc = this-&amp;gt;nfc;&lt;/P&gt;&lt;P&gt;/* Accept the new timing. */&lt;/P&gt;&lt;P&gt;nfc-&amp;gt;timing = *timing;&lt;/P&gt;&lt;P&gt;/* Return success. */&lt;/P&gt;&lt;P&gt;return 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some helps are needed for me to figure this problem out. Thanks very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheng Shi&lt;/P&gt;&lt;P&gt;Emtronix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2012 08:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183948#M8306</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2012-08-27T08:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: how to setup GPMI NAND timing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183949#M8307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sure that no real NAND timing setup is done in gpmi_nfc_hal_v1.c. As there are default settings which can work on most of Nandflash chips, all the nandflash r/w work ok.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2012 09:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183949#M8307</guid>
      <dc:creator>x10</dc:creator>
      <dc:date>2012-08-31T09:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: how to setup GPMI NAND timing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183950#M8308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;yes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But if the EDO mode is enabled with the ONFI nand.&lt;/P&gt;&lt;P&gt;The timing setting will be changed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can read the latest Linus's kernel for reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2012 01:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/how-to-setup-GPMI-NAND-timing/m-p/183950#M8308</guid>
      <dc:creator>HuangShijie</dc:creator>
      <dc:date>2012-10-12T01:49:39Z</dc:date>
    </item>
  </channel>
</rss>