<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Enabling MIPI &amp; Parallel Camera in SabreSD Lollipopp in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-Parallel-Camera-in-SabreSD-Lollipopp/m-p/509993#M83042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We have enabled the support for both MIPI &amp;amp; Parallel Camera in our Customized board which is based on SabreSD design&lt;/P&gt;&lt;P&gt;My question is how can we verify both the camera's working properly&lt;/P&gt;&lt;P&gt;Currently we have verified both Camera functionality using the default camera application present&lt;/P&gt;&lt;P&gt;but that only launches 1 camera (Mipi or Parallel), So we removed 1 camera at a time &amp;amp; tested the other camera functionality&lt;/P&gt;&lt;P&gt;But is there separate Camera applications for launching Both camera's independently&lt;/P&gt;&lt;P&gt;Or is there any patch by which 1 camera application can toggle between both the cameras&lt;/P&gt;&lt;P&gt;Any help is appreciated !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Himanshu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 Apr 2016 19:52:25 GMT</pubDate>
    <dc:creator>himanshugusain</dc:creator>
    <dc:date>2016-04-17T19:52:25Z</dc:date>
    <item>
      <title>Enabling MIPI &amp; Parallel Camera in SabreSD Lollipopp</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-Parallel-Camera-in-SabreSD-Lollipopp/m-p/509993#M83042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We have enabled the support for both MIPI &amp;amp; Parallel Camera in our Customized board which is based on SabreSD design&lt;/P&gt;&lt;P&gt;My question is how can we verify both the camera's working properly&lt;/P&gt;&lt;P&gt;Currently we have verified both Camera functionality using the default camera application present&lt;/P&gt;&lt;P&gt;but that only launches 1 camera (Mipi or Parallel), So we removed 1 camera at a time &amp;amp; tested the other camera functionality&lt;/P&gt;&lt;P&gt;But is there separate Camera applications for launching Both camera's independently&lt;/P&gt;&lt;P&gt;Or is there any patch by which 1 camera application can toggle between both the cameras&lt;/P&gt;&lt;P&gt;Any help is appreciated !!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Himanshu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Apr 2016 19:52:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Enabling-MIPI-Parallel-Camera-in-SabreSD-Lollipopp/m-p/509993#M83042</guid>
      <dc:creator>himanshugusain</dc:creator>
      <dc:date>2016-04-17T19:52:25Z</dc:date>
    </item>
  </channel>
</rss>