<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eMMC interface on I.mx257  in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-interface-on-I-mx257/m-p/509624#M82980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanted to interface eMMC on I.MX257 processor, can anyone please share the information fon doing this?. I also wants the processor should boot from eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Awaiting for the valuable suggestions.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Mahesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Feb 2016 07:49:11 GMT</pubDate>
    <dc:creator>maheshk</dc:creator>
    <dc:date>2016-02-15T07:49:11Z</dc:date>
    <item>
      <title>eMMC interface on I.mx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-interface-on-I-mx257/m-p/509624#M82980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanted to interface eMMC on I.MX257 processor, can anyone please share the information fon doing this?. I also wants the processor should boot from eMMC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Awaiting for the valuable suggestions.&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Mahesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Feb 2016 07:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-interface-on-I-mx257/m-p/509624#M82980</guid>
      <dc:creator>maheshk</dc:creator>
      <dc:date>2016-02-15T07:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC interface on I.mx257</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-interface-on-I-mx257/m-p/509625#M82981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX25 series processors have the Enhanced Secured Digital Host Controller&lt;/P&gt;&lt;P&gt;(eSDHC) interface modules that support the operation of SD/SDIO/MMC/eMMC&lt;/P&gt;&lt;P&gt;devices. For more information, please refer to the Chapter 23 of the i.MX25&lt;/P&gt;&lt;P&gt;Reference Manual Rev.2 document, available on the NXP web site:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx25-processors/multimedia-applications-processors-point-of-sale-pos-robust-security-connectivity-arm9-core:i.MX258?fpsp=1&amp;amp;tab=Documentation_Tab" rel="nofollow"&gt;http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx25-processors/multimedia-applications-processors-point-of-sale-pos-robust-security-connectivity-arm9-core:i.MX258?fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The system boot through the eSDHC interface (in other words, boot from an eMMC&lt;/P&gt;&lt;P&gt;device, connected to the eSDHC interface) is also supported. For more&lt;/P&gt;&lt;P&gt;information, refer to the Chapter 7&amp;nbsp; "System Boot" of the document above.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Feb 2016 07:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-interface-on-I-mx257/m-p/509625#M82981</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2016-02-16T07:40:09Z</dc:date>
    </item>
  </channel>
</rss>