<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Default Console for U-boot - How do I change it?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Default-Console-for-U-boot-How-do-I-change-it/m-p/509515#M82949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved: CONFIG_MXC_UART_BASE must also be changed to the same UART in the board include file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_UART&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#define CONFIG_MXC_UART_BASE UART3_BASE&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_CONSOLE_DEV "ttymxc2"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jan 2016 22:52:42 GMT</pubDate>
    <dc:creator>PaulDeMetrotion</dc:creator>
    <dc:date>2016-01-21T22:52:42Z</dc:date>
    <item>
      <title>Default Console for U-boot - How do I change it?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Default-Console-for-U-boot-How-do-I-change-it/m-p/509514#M82948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to change a Yocto build so that it uses ttymxc2 as the console instead of ttymxc0. I changed the environment variables so that the console is 'console=ttymxc2,115200n8'. When I boot the sd card, the u-boot messages are still output to ttymxc0 and then the kernel messages are output to ttymxc2. Where can I change the u-boot console so that its messages are also output to ttymxc2? Is this not changeable?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 22:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Default-Console-for-U-boot-How-do-I-change-it/m-p/509514#M82948</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2016-01-21T22:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: Default Console for U-boot - How do I change it?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Default-Console-for-U-boot-How-do-I-change-it/m-p/509515#M82949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved: CONFIG_MXC_UART_BASE must also be changed to the same UART in the board include file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_MXC_UART&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#define CONFIG_MXC_UART_BASE UART3_BASE&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_CONSOLE_DEV "ttymxc2"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 22:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Default-Console-for-U-boot-How-do-I-change-it/m-p/509515#M82949</guid>
      <dc:creator>PaulDeMetrotion</dc:creator>
      <dc:date>2016-01-21T22:52:42Z</dc:date>
    </item>
  </channel>
</rss>